Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Power Tool Setter

Power Tool Setter
Sales Price: 5.99 SGD
Review Rating: 4.00
3 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
To fasten the bolts
5
From Japan
On 2018-03-19 00:17:31
I bought it because I often turn 8 mm bolts and nuts. I think that it will be gone without dropping or losing the screw because it can be held securely at the hexagon part of the bolt / nut.
This review is about item#89688645.
With Impact Driver!
2
From Japan
On 2014-07-23 10:23:41
In the steel sticking work on C steel, using the charge impact driver, when the screws were rotated as much as they were, the bearing balls in the holes were lost in the holes. . . .
This review is about item#39505961.
Work tools
5
From Japan
On 2014-02-20 15:24:26
It is useful for screw screws with a necessity tool and it is a repeat purchase, but I would like to keep a spare if it is a little cheaper. . . .
This review is about item#39505961.
1
Customer Who Viewed This Item Also Viewed
Hex Bit Socket
Ring Nut Setter
Nozzle 4 mm
22mm open ring head
Socket Bit MA20S