Customer Reviews of Hex key wrench,long type
|
|
---|
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
During machine maintenance

From Japan
On 2018-01-17 16:15:27
Used for 2.5 hex bolts. I was looking for a long wrench which makes it easier to put in force as it scrapes the head of the bolt.
This review is about item#39522357.
Civil works under construction, for heavy machinery maintenance

From Japan
On 2017-08-26 18:16:58
It is just right length without need of tekipipe. We plan to buy different sizes as well.
This review is about item#39522411.
Replacement for exhaustion

From Japan
On 2016-09-29 16:16:49
It is purchase for on-board mounting for belt squealing. It seems that it can be used without problems by making it solid.
This review is about item#39522411.
Used to loosen screws fixed with locking agent with a flat hand at instantaneous power

From Japan
On 2014-12-05 11:25:42
Impression after using 2.5 ㍉ 3 pieces It will not break easily. On the other hand, with fixed screws, the torque concentrates on the exposed part of the neck length and twists. As the size of the hexagon is crisp, the threaded hole into which the wrench was inserted was never stupid. If it is another expensive product, it may be broken and can not be used if torque is applied, but this product can be used as it is to some extent because no abnormality occurs in the screw insertion part.
This review is about item#39522357.
Joining of hexagon socket screw

From Japan
On 2014-09-14 14:53:45
Because it is not so stuck, it is enough without plating.
This review is about item#39522436.
Alignment of piping

From Japan
On 2014-06-16 08:53:52
I burn the tip and hit it to sharpen it and use it as Sino. Extremely convenient
This review is about item#39522332.
As baked stretching the tip

From Japan
On 2014-03-24 13:27:11
It is different from the original usage but satisfied
This review is about item#39522314.
1