Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Non Adhesive Tape

Non Adhesive Tape
Sales Price: 3.99 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Taping of air conditioning piping
5
From Japan
On 2018-03-20 22:03:48
I am using it for the taping of the air conditioning piping, but it is a good product that is convenient to use.
This review is about item#39539945.
When air conditioner is new, it is used for covering flare piping
3
From Japan
On 2017-05-09 20:21:12
Especially it was able to be used without problems. I did not feel particularly easy to wrap around, but it was a feeling of stretching well.
This review is about item#39539945.
To the winding of air conditioner piping
4
From Japan
On 2016-06-19 22:03:49
Supple and easy to roll
This review is about item#39539963.
Repair
5
From Japan
On 2015-11-28 18:05:57
It was easy to use.
This review is about item#39539954.
Protection of air conditioning piping
5
From Japan
On 2014-06-18 10:28:38
I thought about talking to a construction company because piping tapes of air conditioner was torn up by a large scale renovation work but I decided to repair by myself for about ten years as a lifetime. There seems to be sticky and non-sticky, but sticky one seems to have a longer life, but the durability of the tape itself should not change only by the difference whether it is stuck or not. I thought that it would not be possible to redo if it was sticky, so I purchased non-sticky. I do not know about durability, but I thought that pulling and elongation well quality is good. It also has waterproof because it flickers like a ball when water is applied. I was able to wind around 6 m by one. It was a bit insufficient but it was only a part of the sun that was getting dreadful, so I did it with this. I think that it can not wind even 6 m when taking the overlapping part about half.
This review is about item#39539945.
1
Customer Who Viewed This Item Also Viewed
Adhesive Tape
Non Adhesive Tape
Disc Springs For Light Duty, Stainless Steel
Neopita Tape
Wing Bolt, Stainless Steel
Marking Tape
Non Adhesive Tape
50mm non-stick Kotepu
Light Tuck
Non Adhesive Tape