Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Low-Starting Resistance Wheel

Low-Starting Resistance Wheel
Sales Price: 14.99 SGD
Review Rating: 4.62
8 Customer Reviews
5 star 6
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Repair of product rack etc
5
From Japan
On 2018-02-24 09:58:42
The ground contact area of ​​the tire was small and rolling well. Perhaps the bearing was also good.
This review is about item#39556684.
Karaoke equipment track
5
From Japan
On 2017-12-09 10:44:45
Ordinary steel plate Rubber wound 150 mm Caster 4 pieces attached and used to move the flooring floor by about 10 m, but it did not start easily due to the resistance of the floor and rubber, especially for direction change, It took a considerable force. I bought only low starting wheels. The result is good. I could not convince buying three kinds of casters by type and settled on a low starting caster.
This review is about item#39556684.
When moving a bogie
5
From Japan
On 2017-12-05 16:37:08
I can not say anything because I can not use it much yet, but I think I want to have five years.
This review is about item#39556684.
By craft
5
From Japan
On 2017-05-08 10:58:23
I used the tail wheel of the cultivator for the work, but I think it is very good !!
This review is about item#39556684.
Replacing deteriorated tires
3
From Japan
On 2015-12-03 19:47:31
Is it due to the center bearing? The rotation is not smoother smooth. How about the durability of the rubber covering the wheel? Whether it is good or bad field ..... not hard, so there is no worry about deterioration, there is a possibility of tearing .... Well let's see.
This review is about item#39556684.
For equipment wheel
5
From Japan
On 2015-10-22 15:15:54
If the wheels of a small compressor are broken, if you are looking for a wheel with a small diameter shaft, it is cheap wheels, lightweight · with bearing, so rolling resistance is very low so I am very satisfied with very smooth movement.
This review is about item#39556684.
Create dolly for cutting flowers
5
From Japan
On 2015-05-01 20:13:52
It is a farmer who is making flowers (Turkish Flower). I made a bogie for cutting the flowers and harvesting them. The wheel of the thing which used before was necessary for maintenance such as lubrication without bearing, but this is very low to move because there is only low start to flowing water. However, it is not necessary that the load capacity of one wheel be 200 kg, so I think that there is something lighter.
This review is about item#39556684.
Truck rear wheel
4
From Japan
On 2015-03-01 14:13:01
I was looking for a thing with a shaft diameter, 12 mm (things as thin as possible), wheel diameter, 150 mm or more. The tire which is R is quiet, I like it lightly with the wheel of nylon resin.
This review is about item#39556684.
1