Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Microfiber Mop

Microfiber Mop
Sales Price: 31.62 SGD
Review Rating: 5.00
6 Customer Reviews
5 star 6
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Mop of flooring
5
From Japan
On 2016-12-14 02:08:07
【Composition】 · possession: length can be adjusted. The tip screw is connected to the cross holding part. Cross holding part: With two degrees of freedom, there is a foam member at a part in contact with the cross part. Cross fixing part: rotates with respect to the cross holding part, and the convex rib on the cross fixing part is fitted in the hole in the cross holding part to fix a part of the cloth. Cross (mop): There is a green mop part and a white fixed part (cloth). 【Features】 · While cheap, it is necessary to get dust and dust such as hair often. · Thick resin and metal handles are hard to deflect even when applying force, and can be moped while applying force. - It is an unusual composition that makes the cloth mesh with the cross fixing part, and the cloth never comes off the cross holding part during the mop brushing. It is very convenient. · When removing the cloth from the cross holding part, rotating the cross fixing part, there was a momentum that the injured person got injured. Attention is necessary.
This review is about item#39602586.
House cleaning
5
From Japan
On 2016-10-25 10:04:37
It is used for dry wiping after water wiping mop. I think that it is good to be able to remove the remaining small dust.
This review is about item#39602586.
Inside and outside cleaning
5
From Japan
On 2016-04-26 06:31:05
It can be used indoors and outdoors and I am very satisfied with durability.
This review is about item#39602586.
Experiment
5
From Japan
On 2015-09-01 14:51:17
Please lower the price
This review is about item#39602586.
I am using it to clean the classroom.
5
From Japan
On 2015-08-03 17:11:24
Very light and easy to handle. Since moisture can also be wiped away, it can be used without any trouble. Easy to set up because it is easy to set up. I am not doing the laundry, so I want to see the situation in the future.
This review is about item#39602586.
Cleaning of flooring in the clinic
5
From Japan
On 2013-05-19 01:13:36
Product is satisfactory with quite superior thing that it does not have a problem, it stands still, it can cling with mild power, it can handle clamshell as it is, cloth washing will be beautiful without detergent. However, packing materials when sent are 11 large sheets of cardboard boxes and 50 x 80 cm buffer paper. As a result, we produced a lot of trash. Although polite packaging may be rejoicing, garbage disposal is manual. Since it is an individual business, no new personnel expenses will occur, but there is no difference in manpower. It is time consuming to fold the buffer paper down and throw it away, it's quite a fun. Also, because disposal of business garbage is charged, I think that it took time and disposal expenses to save expenses. Since the contents are cleaning mops and it is not so easily broken, I thought about packing methods once again and wanted to think about the system to collect cardboard even at the time of the next order.
This review is about item#39602586.
1
Customer Who Viewed This Item Also Viewed
Microfiber Gloss Mop Cloth
Flooring Wiper 300
EF moko mop micro 1 pieces
Flat Mop Tool
Light Aluminum Mop
FF rag mop
Micro mop 400
FF rag mop wide II
Protech Microfiber Pad
Floor Mop
Mop
  • Mop
  • TERAMOTO
  • -
Floor Mop
Condor flooring wiper 300