Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Arm Led Magnifier

Arm Led Magnifier
Sales Price: 409.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Model making / Reading
5
From Japan
On 2015-06-22 21:27:21
The contents of the description of the explanation such as the LED preliminary, the presence or absence of other magnification lenses, no guidance on price, etc. are scarce. The strength of the base of the cover is uneasy. Although there are points etc., I want one more place now that the presbyopia became presbyopic price because the price is cheap for the size of the lens.
This review is about item#40178345.
Solder work, work etc.
5
From Japan
On 2015-03-22 00:52:27
Compared with things of about 5000 yen, we purchased this although the price was triple because the lens was big. LED is bright, white is also natural feeling very easy to work. Since it has a switch outside the cover it is easy to use as a desk light. However, the lens diameter of 178 mm of the item description seems to be the size of the lens being used, in fact there is a frame of installation, so the visible part is about 168 mm. Also, since it is made in China, the lens is dirty and plastic burr is left in a new article boxed out condition like normal. Although some people feel that the cover is in the way, I think that it is better not to remove it as it is to prevent the sunlight from being gathered and becoming a fire.
This review is about item#40178345.
Electrical engineering experiment
4
From Japan
On 2014-06-13 13:53:10
The lens is large and easy to use. It is suitable for detailed work such as soldering, although it is not as large as using a stereomicroscope.
This review is about item#40178345.
Soldering work
5
From Japan
On 2014-04-01 14:06:35
I used the same kind of fluorescent light up to now, but I can not go back to using it. The lens is wide, the field of view is wide, the focus quickly fits, bright ... It is very easy to use and easy to use.
This review is about item#40178345.
Crimping of fine parts, soldering and processing, etc.
5
From Japan
On 2014-02-24 12:27:18
Since it is LED light, there is no flicker and the lens is large so we can use the visible range widely so we can reduce eye fatigue.
This review is about item#40178345.
1
Customer Who Viewed This Item Also Viewed
LED Illuminated Magnifier
LED Magnifying Glass
IC Test Clip
Led Lighting Magnifier
Light Loupe
56LED Flexible Arm Magnifier
L-Zoom Arm Light
80LED Flexible Arm Magnifier