Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hook Wrench

Hook Wrench
Sales Price: 28.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 5
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Motorcycle Maintenance
5
From Japan
On 2018-01-16 15:42:29
It is a light and easy to use product. Since angle is good, it can be used in various scenes!
Motorcycle maintenance
3
From Japan
On 2018-01-04 19:57:26
It can be adjusted, so it's reasonably convenient. It's cheap.
This review is about item#40280904.
Motorcycle Maintenance
5
From Japan
On 2016-08-05 16:21:48
It was a very easy-to-use and satisfactory product. The hook's hook was also good and the force was easy to hang.
This review is about item#40280904.
bike
5
From Japan
On 2016-04-16 23:47:34
It is used for tightening the K50's exhaust pipe. Although the hook moves freely, it was able to hold firmly at the time of work. I think that the hold feel is the same as the exclusive size. Since construction is solid, it seems necessary to check well whether it can be used in a narrow place,
This review is about item#40280904.
Rear suspension adjustment of motorcycle
5
From Japan
On 2015-12-18 15:34:16
Since it was used in a narrow recessed place, I could not use it unless the handle of the claw finally finally grabbed the terminal of the handle with a monkey and extended while changing the angle, but if you use it normally I think that there is nothing wrong. The reason for choosing this product was that I could adjust it because I did not know the size, and it seemed that the price was reasonable. I was worried about the thickness, but if you make it thin, the unit price will also rise. I think that it is a good product in terms of price.
This review is about item#40280904.
Adjustment of bike stem removal and rear shock spring adjustment
5
From Japan
On 2015-01-12 15:59:50
Adjustment of the spring of the mini diameter stem and rear shock of about 50-100 cc was done without any problem. Although I think there are some cheap items, I thought that there is no mistake if it is a motorcycle manufacturer for the time being, purchase. As a result, I can adjust the size and it seems to be used for almost anything.
This review is about item#40280904.
Maintenance of motorcycle
3
From Japan
On 2014-05-05 13:50:58
It is possible to improve usability in various scenes when it can be made variable so that it can be attached with resistance.
This review is about item#40280904.
1
Customer Who Viewed This Item Also Viewed
Connection spanner
FP hook pin spanner
45-52mm Hook Wrench
Freely hook wrench
25-28mm Hook Wrench
Flexible hook wrench
Pin Spanner
Sliding adjustment hook spanner
Hook Spanner
Adjustable hook wrench