Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wall Access Hole

Wall Access Hole
Sales Price: 24.99 SGD
Review Rating: 3.50
6 Customer Reviews
5 star 1
4 star 3
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Wood work
4
From Japan
On 2018-02-27 19:42:41
It has good workability and is easy to use so I think I will purchase again.
This review is about item#40358491.
For cat's mouth
4
From Japan
On 2016-12-25 13:17:50
Just drilling a hole in the board makes it look poor, so we wrapped the frame and made a nice looking port for the cat.
This review is about item#40358464.
I installed it on the wall of the duct for wiring at home.
4
From Japan
On 2016-04-26 22:43:40
The structure is the same as the one with a width of 20 cm, but it seems to be slightly inferior in terms of accuracy. The gap between the opening and closing door and the frame was bigger than I thought (about 2 mm), so I was a little worried, so I made it four stars.
This review is about item#40358421.
As an inspection port
1
From Japan
On 2016-03-05 12:49:36
I bought six pieces, but there were three big dent scratches. The probability of 1/2 is Saiak. It was something that I could see enough when packing up.
This review is about item#40358464.
Building interior refurbishment
5
From Japan
On 2014-04-04 16:56:02
I am firm and very satisfied.
This review is about item#40358421.
In the inspection hole of the wall
3
From Japan
On 2012-10-30 22:22:21
For WE 25 J type, the screw holes to hold the outer frame are 1 above, left, and right, respectively. Somehow I am not free. Although it may be as small as 250 corners at three places, it may not be a problem if it is not frequently opened and closed, but it is cluttered that when the leaf springs on the outer frame interfere with the inner frame and the tension is As it seems to be so, there is a slightly glad feeling when locking and tightening. The goods are solid in both the inner frame outer frame and the rhombus. As expected it is made by Daiken.
This review is about item#40358421.
1
Customer Who Viewed This Item Also Viewed
Home Wall Access Port
Pvc Ceiling Hatche
Access Panel Frame
Meter Inspection Hole