Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hexagon Bolt With A Hole, Scm435 / Black Oxide Film WithFine Thread

Hexagon Bolt With A Hole, Scm435 / Black Oxide Film WithFine Thread
Sales Price: 9.99 SGD
Review Rating: 3.62
8 Customer Reviews
5 star 3
4 star 1
3 star 3
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
anything
3
From Japan
On 2016-04-25 01:57:29
The surface treatment of the bolt is probably black stain, that is, it is considered to be only black stain on the SCM material fabric. I rust. There are UNIQLO, chromate, other surface treatments if you consider rust prevention. But the other one is rusty. I think that the surface treated bolt suitable for the purpose of use is good. Even if it is screwed in by other person, it is unpleasant as it can not be screwed to the base of the head of the cap bolt. Normally there is no usual use of a washer or a combination of lock washer and taper washer dedicated to cap bolt. Since there are quite a variety of suitable positions and methods of use, we recommend that you are recommending "Screw list" so it is surprisingly cheap, so you better purchase it and increase your knowledge, you should also upgrade yourself. It is difficult to close the vault relationship. It is recommended to carefully examine materials and hardness etc. (although surface treatment is also true). I would be pleased if you could refer.
This review is about item#40377863.
Automobile Restore
5
From Japan
On 2016-02-26 19:24:01
Automotive bolts (detailed items) are saved because there are few stocks at home centers. Recently the number of automobile parts store in town has decreased, and the place where we have inventory of bolts has become less
This review is about item#40377802.
Attached to a car
1
From Japan
On 2015-06-01 17:47:02
Black oxide film rusted with rain twice, not problems like having a month or not. I think it is false because of my experience! I can not trust that it really uses SCM material if this quality is ...
This review is about item#40377793.
Automotive applications
5
From Japan
On 2015-04-01 20:06:30
It is very firm and has strength as well. If the price is easy and the amount is large, it is saved,
This review is about item#40377802.
Part assembly
3
From Japan
On 2014-12-04 23:57:13
I bought M12 × 40, but since there is no screw thread at the root as much as 3 mm, a spring washer or washer is necessary. It was unsuitable for use to fix with just this screw.
This review is about item#40377863.
Bicycle crankshaft
5
From Japan
On 2012-12-17 14:59:21
I have not used it, but I am satisfied.
This review is about item#40376402.
Using a motorcycle
4
From Japan
On 2012-11-03 19:30:46
In addition to all screws, I would like you to sell half screws and one piece from one.
This review is about item#40377872.
I use it for a motorcycle
3
From Japan
On 2012-05-30 16:51:26
The detailed threads are saved because they are not readily available. Just because it costs a shipping cost ... It is expensive if it is a small amount.
This review is about item#40377784.
1