Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Sliding Door Roller Window Sash

Sliding Door Roller Window Sash
Sales Price: 11.99 SGD
Review Rating: 3.90
10 Customer Reviews
5 star 5
4 star 1
3 star 3
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Because of poor movement of the door roller,
3
From Japan
On 2018-04-08 20:02:28
Since I bought it at the home center before, I searched it on the tablet. I was saved because it was in a monotail. I installed it immediately. I was happy with the quick correspondence. (^ o ^)
This review is about item#40410246.
Exchange of old aluminum entrance sash door roller
3
From Japan
On 2017-08-07 16:43:03
We exchanged aluminum front door with this type 20 years ago. I had difficulty in removing old door roller. It is a momentum to break. (Maybe there are tricks?) The size was perfect, but it was easy to get out, and it was hard to put it down when put in the rail. I wish I could fix it snugly. When the door is removed, the door roller falls and it gets caught between the sash and the rail, I think that it is difficult to remove the door. I think that it depends on the shape of the entrance door lower part, too? After exchanging for fluffy movement is comfortable to move smoothly.
This review is about item#40410246.
Door entrance sliding doors, entrance-like wind-free door
4
From Japan
On 2017-06-04 07:36:09
There are no problems with using some of them for testing, but when the adjustment holes of the screws do not match, you have to adjust and remove them so I want you to devise
This review is about item#40410246.
Exchange of sashed door roller
1
From Japan
On 2017-02-06 21:11:28
Four pieces are used for sash of width 1800. I confirmed conformity width, depth and load and thought that it was conforming, but the spring did not work and it got in the back of the sashi. As a result, I could not fulfill my duties and replaced it with another car. I think that the cause can not bear the spring. Not suitable for 4 use? I think that it should be verified and improved.
This review is about item#40410246.
Exchange broken door roller
5
From Japan
On 2016-08-10 17:54:29
Easy to replace, the door became very light.
This review is about item#40410246.
Exchange doorway at the entrance
5
From Japan
On 2015-05-04 10:05:14
It was easy to install because it was an inlay type. How much longer is there to have it. I am satisfied if it brings it for about 10 years.
This review is about item#40410237.
Exchange of door sliding door of aluminum sliding door
5
From Japan
On 2014-08-05 13:47:07
Special items and other items are greatly appreciated. I could purchase it much cheaply as compared with the home center. Although durability is undecided, I think that it is a sufficient product as it is a consumable item.
This review is about item#40410246.
Periodic replacement of consumables
5
From Japan
On 2014-06-23 18:54:31
I was looking for a roller car sliding door painfully. There was no compatible item in the home center, but I had a hard time, but the item description was easy to understand, and I could purchase it at a lower price than the home center.
This review is about item#40410246.
Exchange of the door of the entrance sliding door
3
From Japan
On 2013-09-20 12:22:50
Mounting is easy. There is no problem with adjusting the height. Just because the diameter of the car is small, or because there are no bearings on the shaft, movement can not be said to be smooth. I wonder if it is spinning. Silicon oil sprayed, but there is no rattling but movement is rather heavy.
This review is about item#40410237.
Replacement of aluminum sash doors
5
From Japan
On 2013-09-08 22:45:19
Due to the rust of the door roller, I decided to purchase because the opening and closing of the sash was no longer smooth. Usually it is normal to ask the merchant, but since I had solved the exchange procedure, I was very satisfied because I was considering purchasing from the cheapest possible place.
This review is about item#40410246.
1