Customer Reviews of LED Flashlight,Rain-Proof Outdoor Type,For Both Of 100V/200V
|
Sales Price: 189.99 SGD
Review Rating:
![]() 4 Customer Reviews
|
|
---|
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Temporary lighting outdoors

From Japan
On 2018-03-28 12:39:01
There is no problem as ability as a lighting fixture, but in this package
Foot for lighting independence is optional and not included.
Although the model number of the foot for putting on the floor is LEN - S, it seems that there is no handling in the monotalou.
This review is about item#40420265.
Light up an outdoor sign

From Japan
On 2015-11-19 19:05:05
I like the way the lights are growing like I got a line.
This review is about item#40420265.
It is used as a substitute for a signboard light (halogen 150 W).

From Japan
On 2014-06-23 12:48:02
We installed as a substitute for both mouth halogen 150W. It delivers illuminance comparable with power consumption of 11.2 W and 1/13 power. It can be used instead of spot lighting. 1. Ultraviolet rays are almost 0 and sunburn does not occur. 2. It will not get hot. 3. Insects do not come. 4. Durability: It is likely to recover quickly with an electricity bill that is more than 10 times cheaper than the cost.
This review is about item#40420274.
Watching garden trees and flowers light up

From Japan
On 2014-04-10 16:28:43
Purchased according to the flowering of Yoshino cherry tree in the garden. I was lighting up using LED light bulb equivalent of 60 watts, but it was dark now ... I purchased this product. Because the illuminance was high, I could light up the whole tree of cherry blossoms. Future season ... Since trees will bloom one after another, we are planning to change the subject of light up successively. Then, it is safe and good to have drip-proof specification.
This review is about item#40420265.
1