Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Arm Stopper

Arm Stopper
Sales Price: 28.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 6
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
When the door stopper can not be attached to the floor
5
From Japan
On 2016-12-12 19:02:16
Because of the price, it is a solid product, this time purchased by repeat. It is greatly appreciated even at the work site because the delivery schedule quickly enters.
This review is about item#40982785.
For new interior doors
5
From Japan
On 2016-03-07 18:42:26
I forgot to order the door stopper at the time of ordering the fittings, and in a panic, I found it here and ordered it. Since I chose a pon attachment type, there is no particular problem in installation. It arrived in a day and it was saved.
This review is about item#40982785.
As a simple fixation of aluminum opening doors
5
From Japan
On 2015-12-25 14:52:10
Since I work with the door open, I used door checks until now, but because it breaks well, I thought of a good way. The arm stopper of this time is easy to install, it is inexpensive It is enough.
This review is about item#40982785.
3 story prevention door fluttering prevention
5
From Japan
On 2015-10-19 15:04:20
Easy to install, the use feeling was as expected.
This review is about item#40982785.
Door stopper
5
From Japan
On 2014-11-13 15:47:36
There was no stopper at the door and I hit the wall, so I thought about stoppers to attach to the wall but I purchased it here. It was easy to install, because the door of the house was a solid tree, it became screw tightening after drilling a hole with a drill, but it is simple, it does not go beyond the MAX value properly and there is a little spring so the door There is no thing like being shaky. Conversely, even if a strong wind blows, I feel satisfied that it did not close with Butterne. Here is a high reception type, you can put on the upper part of the door, so if it is a house with only the thickness of the door it will not be attached. I wonder if there is such a house. I would be happy if you could put a little more variation if you wanted greed.
This review is about item#40982785.
Door stopper
5
From Japan
On 2014-06-15 14:49:22
There is no problem with the price. There is no problem with the degree of opening and closing by the manual reasoning dimension. There is no problem if you purchase it by looking at the drawing dimension with high acceptance.
This review is about item#40982785.
Mansion renovation
3
From Japan
On 2014-03-24 15:58:50
I bought it because the model number of this product itself is 312 type. It was different from the one on site. There are different things such as "high reception type", "surface type", "excavation type", etc. after the 312 type of this product, which is the cause of the confirmation mistake here. There was no big problem because it was installed at a position different from the original screw hole, but if possible, make installable parts replaceable so that the mounting height can be changed on site, or if the number of the model number itself is changed to "312 It was not like a derived type of "I felt that it would be more wrong to assign individual numbers to each one. Product, operation itself is good.
This review is about item#40982785.
1
Customer Who Viewed This Item Also Viewed
Stainless Arm Stopper
Door Arm
Iron Arm Stopper
Stop stay
Stainless Arm Stopper
Adjustable Stays
Stainless Stays
Door Arm
With arm stopper face
Stainless Arm Stopper