Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Steel Reinforcing Corner Bracket

Stainless Steel Reinforcing Corner Bracket
Sales Price: 1.99 SGD
Review Rating: 4.60
10 Customer Reviews
5 star 7
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
When creating oven setting stand
5
From Japan
On 2018-03-18 21:17:33
It was nice to really order. Until we sent it was half-trusted but it was more than ideal item. Thank you.
This review is about item#40986242.
Socket fixing of fluorescent light type LED light
5
From Japan
On 2017-11-27 23:25:52
I used it for socket fixing of one side electrode type LED light. This type of light is attached directly to the ceiling frame with only a socket, but I am satisfied that it can be installed smartly with the smallest size that is inconspicuous. When inserting a rodlike light between sockets, it is necessary to compress the spring, but strength was also sufficient.
This review is about item#40986251.
Penetration of stone walls
4
From Japan
On 2017-10-22 17:50:22
I purchased it because it is cheap because there is no screw. If you choose the screw according to the application with strength, it is used in various places.
This review is about item#40986251.
To prevent slippage of the shelf board
3
From Japan
On 2017-08-14 12:23:08
This time I bought it to stop the shelf board. It was good with cheap things, but it happened to be pretty robust so it happened somewhat hesitated, but I chose this because I did not feel like buying a thin thing high. As you can see in other reviews, the screw hole is big. (Screws are not included) When I measured it with a caliper, there seems to be a diameter of 4.5 mm. Since there were no screws of 4.5 mm at hand, I do not know whether or not to pass. I passed the screw of M4 with enough margin. The screw hole is inclined so that the countersunk head can be accommodated from either side of the front or back. As I tried several meetings, I think that it can be used because the countersunk head of the tapping screw of M3 gets in and does not fall out. The 3.5 mm wooden screw tray will protrude slightly without being fitted. I thought the dish head of the 3.1 mm wood screw just exactly, but it will slightly protrude by 0.1 or 0.2 mm.
This review is about item#40986242.
Reinforcement of wood connection
5
From Japan
On 2017-06-27 17:21:46
I use it without any problems. It is quick and cheap and I am grateful.
This review is about item#40986251.
Reinforcement of furniture
4
From Japan
On 2017-03-29 20:47:42
It was good for the price and it was solid. Though the screw hole is bigger than I expected, there was no problem with use. Cost performance is good. However, it is cheap, so shipping costs become a problem.
This review is about item#40986242.
Linking
5
From Japan
On 2016-05-02 22:24:56
It was thin, durable and easy to use
This review is about item#40986267.
For consolidation
5
From Japan
On 2015-12-11 01:57:50
It is a very beautiful item.
This review is about item#40986242.
Wood working
5
From Japan
On 2015-11-06 07:00:33
The item arrived immediately.
This review is about item#40986242.
As a general purpose hardware
5
From Japan
On 2015-10-12 21:32:21
It is cheap and satisfactory. There is no problem in quality.
This review is about item#40986251.
1