Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Takobo SET

Takobo SET
Sales Price: 15.99 SGD
Review Rating: 4.00
8 Customer Reviews
5 star 4
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
K 6 A to OH
5
From Japan
On 2018-04-29 08:08:46
Convenient with two types of coarse and fine compound. Because it becomes an amount which can not be used when purchasing with compound alone.
This review is about item#41449143.
Engine Overhaul
4
From Japan
On 2017-05-20 21:31:38
It was able to be used enough for the balancing of 16 valves. I think that I can not endure professional use, but this level is enough if it is about one engine.
This review is about item#41449143.
Rubbing the valve seat
5
From Japan
On 2017-03-10 15:40:03
There is no reason to rub the valves something, so this amount was enough.
This review is about item#41449143.
Balancing of off-road motorcycle
5
From Japan
On 2017-01-17 19:32:31
The sticking of the sucker is also good, the feel of the hand is also easy to use well.
This review is about item#41449143.
Motorcycle engine OH
2
From Japan
On 2015-11-24 19:35:47
No no ... Suction power is too little
This review is about item#41449143.
Attach per bulb
3
From Japan
On 2015-10-26 20:43:03
Not suitable for forged surface valves
This review is about item#41449143.
Rubbing cam valves
5
From Japan
On 2015-09-11 20:33:38
Especially there is no problem but I am happy if there is more adsorption power
This review is about item#41449143.
Engine overhaul of motorcycle
3
From Japan
On 2015-04-13 15:32:19
The adsorption on the exhaust side of the valve was bad and the work did not progress. There is no problem on the intake side. It may be caused by the dirt of the valve not falling clean. The compound is sufficient, and it seems that it can be used many times yet.
This review is about item#41449143.
1
Customer Who Viewed This Item Also Viewed
Valve Compound, Carborundum
Repair Suction Cup
Valve Wrapper, Kite Bar
Valve Cotter Mounting Tool
Suction Cup Rod
Valve Lapper
Enamel coffee pot
Valve wrapper
Valve compound
Valve Spring Compressor Set
Valve compound (Chuume)
Valve compound (Saime)