Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flanged-Button Head Screw

Flanged-Button Head Screw
Sales Price: 4.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
When the motorcycle is maintained
5
From Japan
On 2018-05-16 23:39:14
We do not sell this type of bolt easily, so it will be saved.
This review is about item#41486961.
Motorcycle parts installation
5
From Japan
On 2018-03-25 22:49:08
Because it is a lineup which is not put in the home center, it is saved. Since it can be mounted with a nice feel without a washer, the serviceability has improved.
This review is about item#41487074.
When remodeling the outside seat rail of a car
5
From Japan
On 2017-08-18 14:00:52
It was used when remodeling to correct the offset of the seat rail to the door side. Because the depth of the hexagonal hole is shallow, it will be easy to lick the hexagonal hole when tightening · loosen, so it seems better to think about the tool selection to use well.
This review is about item#41487092.
For motorcycles
5
From Japan
On 2017-07-18 18:59:45
For seat cowl mounting. It is easier to tighten because it is a hexagonal change from a cross-shaped screw. I endow with subdivision.
This review is about item#41487013.
Used to re-ground the old car.
5
From Japan
On 2016-08-05 16:04:26
I used it in the ground to the engine block · head, but I think that there is a thing processed to prevent loosening due to temperature rise and aluminum · iron due to the difference in expansion rate. I use the tag with an umbrella part and use it.
This review is about item#41486977.
1