Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hex Socket Button Head Bolt, UNC Stainless Steel

Hex Socket Button Head Bolt, UNC Stainless Steel
Sales Price: 4.99 SGD
Review Rating: 5.00
3 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Bolt replacement for furniture
5
From Japan
On 2016-12-14 20:14:30
The hexagonal hole of the bolt fixing the unit shelf shelf to the scallop of the MUJI made MUJI made goods (not of course advertisement, for the sake of the reader's sake, not to be bad) collapsed inadvertently, this is screw Zaurus Someday I was looking for a substitute because it was necessary to exchange as either. The standard of this bolt is UNC (coarse grid of unified screws) rather than ordinary one ISO (metric screw) (The adjuster bolt is ISO M8,,,,,). Nominal diameter of screw is # 10, length is 5/8 inch, that is, # 10 X 5/8 is correct bolt and head is low, preferably stainless steel is necessary, but naturally such a niche is in the home center There is not. It is always appreciated from the viewpoint of shipping cost and trouble that you can always ask along with other products from the list that is easy to see. When we judged and compare the hand screws and ruler and screw specification table while judging it, I am fortunate correct answer. However, since the unit shelf original bolt has a flange, it can be used for stopping the shelf as it is, but this product has no flange (as long as the low head stainless steel unified screw with flange is checked on the net, unfortunately it is not on the market So), you must bite the washer so that your head does not get stuck in a stupid hole. People without washers, let's buy them here. Also, do not forget to prepare a hexagon socket wrench as the size of the hexagon socket is 3.5 mm smaller than the original (hexagon socket flank width 4 mm). Well, if you are watching this, you already have it ....
This review is about item#41496831.
Maintenance of tape recorder AG-440B made by US AMPEX
5
From Japan
On 2016-08-03 17:13:57
Basically, when assembling after disassembly and repair, screws always use new articles, but old screws had rust a little, so all new screws are stainless steel. The screws purchased this time are satisfactory in terms of accuracy and strength.
This review is about item#41496822.
Repair of old American made chain saw
5
From Japan
On 2015-01-29 09:10:23
It was saved because the size which is not in the neighboring home center was able to purchase from a small amount.
This review is about item#41496822.
1