Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of TRX Countersunk Machine Head Screw, Flat, Stainless Steel, Pack Product

TRX Countersunk Machine Head Screw, Flat, Stainless Steel, Pack Product
Sales Price: 4.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Used for fixing the LM rail of the milling machine
4
From Japan
On 2018-04-29 10:32:02
PB screw products were difficult to find easily under M3. The block side of the LM rail should have 2.30 on the M2, but there is no pack selling is a drawback. This screw was saved by pack sale. The thinner it gets, the less the type it is, it is inconvenient that you can only buy it in thousands of units if you only have box sales.
This review is about item#41748603.
Axis top plate stopper
5
From Japan
On 2018-03-09 14:31:43
Quality could be used without any problem. Because it is a stainless steel screw, it is good not to rust.
This review is about item#41748743.
For fixing the license plate of the car
5
From Japan
On 2017-02-12 20:24:29
In combination with the SUS rosette washer, it was used for fixing the license plate of the car. The bolt attached first rusts immediately, and yellow plating is cheap. Because it is SUS, it is hard to rust and I think it will be useful for preventing theft.
This review is about item#41748935.
Prevent tampering with number plate
5
From Japan
On 2016-04-16 07:22:04
Although I was looking for the same thing locally, I could not find it easily and looked at your TV commercials, I searched the net and found the desired one, I ordered immediately. I think that there is an opportunity to use again with overwhelming product lineup.
This review is about item#41748917.
Replacement of motorcycle brake oil reservoir tank cap screw
4
From Japan
On 2015-08-18 06:24:26
It is good that there is no appearance effect and that you will lick the head of the screw. I examined it in hexagon or Torx, but I did it for Torx this time.
This review is about item#41748734.
Used for license plate of car
5
From Japan
On 2014-09-18 14:59:10
Put the rosette washer and use M6 x 15 mm for the car license plate and M 6 x 12 mm for the two wheel number plate. When using the license plate base with two wheels, please set it to 15 mm. I can not reach the lock nut.
This review is about item#41748917.
Used as a screw to stop the lid of the Nissin brake master
5
From Japan
On 2014-02-14 12:00:02
Used as a brake master of Honda Fusion. It becomes an alternative to 93600-04012-0 G. It also prevents mischief and it also becomes an accent, so the screw is rusty or if your head is collapsing, can you order this and exchange it? The price is also not much different from the original thread two pieces.
This review is about item#41748734.
1