Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of ECO-BS Knurled Screw, Brass, Low Cadmium Material, Chrome Plating, Pack Product

ECO-BS Knurled Screw, Brass, Low Cadmium Material, Chrome Plating, Pack Product
5 star 3
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Motorcycle maintenance
5
From Japan
On 2016-11-09 00:26:02
Unlike plastic, there is a high-class feeling, it is exactly easy to rotate the size of the knob part slightly larger.
This review is about item#41743387.
Used as a substitute for the fine adjustment screw of the high / low adjustment part
5
From Japan
On 2016-08-16 22:33:10
It is generally satisfactory, but because the diameter of the knob portion of the original product is a bit smaller (7 Φ), it would be good if there was variation in size. In addition to chrome plating, there are also color variations such as black paint and gold color.
This review is about item#41743387.
As a prototype part of my work
3
From Japan
On 2016-02-12 10:56:15
Well, because it is just a knurled screw, it is extraordinarily normal without product being possible. To be honest, the unit price is too high in the monotail, so it will be much cheaper to mass-produce from the screw specialty point during mass production. It is useful if you need only a few like this one.
This review is about item#41743484.
Fixation of jig
5
From Japan
On 2013-11-18 13:41:51
It is better to increase the types of knurled screws
This review is about item#41743396.
For fixing parts
3
From Japan
On 2013-02-16 11:33:28
It was good because the price is cheap and it is not inferior to other manufacturers. The shipping fee is cheap, and since the troublesome when ordering is small, it seems to be available from now on.
This review is about item#41743344.
1