Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Joint Clip, General Type, Stainless Steel

Joint Clip, General Type, Stainless Steel
Sales Price: 4.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 4
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Used for outdoor laundry clothes pipe
4
From Japan
On 2017-11-23 21:41:37
To prevent the hanger attached to the clothespin from being displaced by the wind, purchase two or more kinds of different sizes. Originally the rod also had a slip stop attached, but since both ends were missing, I attached it. However, the installation on the pipe was rather hard, and the stainless rolled pipe was scratched.
This review is about item#42090772.
Faucet water supply pipe connection
5
From Japan
On 2017-10-11 14:41:11
It is a special part so it is not easy to get it elsewhere, so it was saved!
This review is about item#42090736.
I used it to fix the smoke cylinder of the car
5
From Japan
On 2017-04-04 15:06:34
Since there is a burr, it was removed with a bit of file, but it is satisfying because it is easy.
This review is about item#42090806.
For storage of tools
3
From Japan
On 2017-03-15 17:53:20
I bought it to catch a stick of 10 mm. Since it was two pieces to use, it would be even better if you sell it in smaller pieces ...
This review is about item#42090711.
System kitchen faucet connection (fixed)
4
From Japan
On 2016-11-17 16:03:37
For model kitchen re-installation system kitchen re-construction, it should have been attached to the attached faucet with zipper, but removal worker seems to have been lost, difficult to obtain, faucet manufacturers unless it is set with check valve parts supply I was in trouble because I did not (4000 yen for parts cost + tax). It is sold here and various sizes are available, and we measured the dimensions of the actual fittings and ordered them to fit. When the parts arrived, it was a great help with the perfect size and shape once you tried using it. The shape + dimensions are also displayed finely, so we have made an accurate order. If there was resin fastener lock (detachment of quick fastener), it was "satisfactory", but because the lock is handmade, it will be rice cake.
This review is about item#42090736.
Base foot holder
5
From Japan
On 2015-11-17 20:41:14
I was surprised to have all these fine items.
This review is about item#42090754.
Pipe fixing
5
From Japan
On 2015-05-04 21:44:26
Stainless steel spring material (with weak magnetism), it seems to be used outdoors.
This review is about item#42090745.
1
Customer Who Viewed This Item Also Viewed
Lights Up And Catches
24 mm spring clip
Fixed holder phi30
Fastener Clip
Fasteners Fittings
Negurokku (spring clip)
Saddle Band
Spring Band Hook
Support Band
Joint clip S type (stainless steel) (small box)
Spring clip
Scoop stop