Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of High Nut, Iron

High Nut, Iron
Sales Price: 4.99 SGD
Review Rating: 4.59
29 Customer Reviews
5 star 23
4 star 1
3 star 4
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 29 Reviews
I used it for bike processing.
5
From Japan
On 2018-04-23 18:45:22
Monotaro that finds what you want! Thank you very much and thank you.
This review is about item#42111912.
It is used to adjust the height of the tread of the stairs.
5
From Japan
On 2018-03-20 11:11:44
Because I do not have the desired length of countersunk screws, I use it as both height adjustment and fixation, but I do not think so much I am satisfied because the effect is out.
This review is about item#42112016.
17 mm female hex detached
5
From Japan
On 2017-11-14 15:51:39
Although it is a wicked way of use, I used it to tighten the 17 mm female hexagon in the back place. It was much cheaper than buying a hexagon stick wrench or a ratchet socket.
This review is about item#42111921.
Used for remodeling so that it can be attached to a car pantograph jack and work with a box wrench or impact
3
From Japan
On 2017-10-23 21:29:24
Actually I do not need an internal thread, but it was too long because it was a hexagonal bar. I would appreciate it if you cut bar steel with a strip cut size.
This review is about item#42111973.
Tool making
5
From Japan
On 2017-07-14 18:30:39
In combination with adjuster bolt and angle steel, we made the tool. There is no problem at all.
This review is about item#42112086.
Motorcycle Parts Installation
5
From Japan
On 2017-06-28 09:37:47
Since it is made of iron, it can be used by welding it to a steel motorcycle frame, so it is convenient when installing parts.
This review is about item#42111876.
Used in combination with a long bolt for the upper and lower bench
5
From Japan
On 2017-03-28 14:59:38
The finish of the screw part can be welded to the steel plate and it is also cleaned cleanly.
This review is about item#42112061.
Tightening the screw in the deep hole
5
From Japan
On 2017-03-16 21:25:30
There is no variation, the quality is good. I can use it with confidence, so I will also buy it next time.
This review is about item#42111727.
Work
5
From Japan
On 2017-03-02 20:42:49
Because it is painted after welding, those of cloth are easy to paint pretreatment. It's good because there are so many sizes.
This review is about item#42111806.
For height adjustment
5
From Japan
On 2017-02-27 04:20:08
I did not scrape because the height was aligned in small increments.
This review is about item#42111797.
To fix the battery.
5
From Japan
On 2017-02-12 22:40:08
It is short because it is a nut attached to the battery, so it is hard to work and replaced. It became very easy to use.
This review is about item#42111736.
To extend the damper of the car
5
From Japan
On 2016-08-16 07:41:46
There was not this size in the home center, it was saved.
This review is about item#42111991.
Protection of screw threads when plating stud bolts
4
From Japan
On 2016-07-19 08:23:11
I chose the one that was cheapest, which was it. I think that it was good because there was no problem.
This review is about item#42111702.
After construction anchor
5
From Japan
On 2016-06-17 15:34:41
I was sorry to have sent you very much urgently.
This review is about item#42112253.
For height adjustment
5
From Japan
On 2016-01-12 18:29:58
The satisfaction level of the finish is a little afterward.
This review is about item#42111684.
Joint
5
From Japan
On 2016-01-11 16:09:04
No problem
This review is about item#42111754.
Car suspension
5
From Japan
On 2015-11-18 21:46:32
It is a cheap and durable safe product.
This review is about item#42112016.
As a T slot bolt nut
5
From Japan
On 2015-11-04 16:22:04
About one-third of genuine parts, it is cheap.
This review is about item#42111946.
Jig for product production
5
From Japan
On 2015-10-14 18:57:23
It was used to make jigs for product production. Iron fabric is useful because it is welded to steel flat bars and angle materials. Both length and thickness are saved a lot.
This review is about item#42111815.
Mount Production
5
From Japan
On 2015-08-18 17:08:56
Good shopping was made.
This review is about item#42111876.
1 2
Customer Who Viewed This Item Also Viewed
Long Nut
Coupling Nut
Coupling Nut
Long Hexagon Nut
High Nut
High Nut
Coupling Nut, Stainless Steel
Coupling Nut
High nut wit (iron / cloth)
High Nut, Iron Chromate