Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hex Nut

Hex Nut
Sales Price: 4.99 SGD
Review Rating: 4.75
4 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Parts of agricultural machinery
From Japan
On 2018-02-28 23:04:10
It is a part of agricultural machinery, but strength and precision are sufficient for this.
This review is about item#42214654.
Maintenance of farm equipment
From Japan
On 2017-09-02 12:27:20
Because it takes time and effort to search for plated high-strength items in the near field, it is very easy to order on the net, there is nothing wrong with the product,
This review is about item#42214697.
Repair of construction machine
From Japan
On 2016-01-28 15:17:56
S45C is mandatory as strength is required. Since painted parts are also plated, it saves you the trouble of re-painting.
This review is about item#42214654.
It is very small, but it is used for installing equipment that always generates vibration.
From Japan
On 2014-03-24 13:13:53
There is a necessity of 5 MM by all means, use a nut and a disc spring which can tighten than a general screw. The thing which turned out after finishing the use almost for a month is as follows. 1. As fast as 7N, there is no thread break, as expected. Use is tightened at 6N. 2. I purchased and used the stain disc spring this time, but it is somewhat disappointing. Compared to the iron disc springs that have been purchased before, it is easier to loosen and needs to be tightened once a week. I would like to handle both iron dish spring CAP · BOLT. Accessories for 5 MM screws are not handled at ordinary screw dealers, and MONOTARO which can be sold as a bulk has enough presence even just that.
This review is about item#42214636.