Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Saddle Band

Saddle Band
Sales Price: 0.99 SGD
Review Rating: 5.00
2 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Fixing of Flexible pipe T type for water supply (G13)
5
From Japan
On 2017-08-08 22:37:01
It was a perfect product for the purpose "to fix the flexure with a little floating from the wall." There are grooves connecting the saddle bands, and pipes can be installed in parallel at very close intervals. Even if the head of the countersunk screw is 9 mm, there are also large holes and depths that can be offset. Beyond imagination, I could fix the flexi. I have to pull a little if I think about going out and it will not come off. I think that it is even better if there is a hole so that the insulock can be passed through in a place to be tightened more firmly.
This review is about item#44382186.
I am intelligent in fixing the simple water piping that depends on flexibility.
5
From Japan
On 2016-07-22 17:27:19
There is a gap in the band formula, it is impossible to lay straight.
This review is about item#44382186.
1
Customer Who Viewed This Item Also Viewed
Lights Up And Catches
Saddle Band
Casing Tube Saddle
Spring clip
PP Saddle for Vp
Pipe holder
click
24 mm spring clip
Connected Saddle Band
Fixed holder phi30
Resin made saddle band
Support Band
Negurokku (spring clip)
Round bar grip