Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Insulating coating with crimping terminal (TG TC type) bar-shaped

Insulating coating with crimping terminal (TG TC type) bar-shaped
Sales Price: 12.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Equipment wiring: For connecting the power supply line to the terminal block on the board.
2
From Japan
On 2018-03-02 10:10:18
Although I talked about when ordering in January, I came as a perforated seal of the seal sealing the package. Just to be sure I counted it by 99 books, one missing item. Although I used it as it was because it was troublesome, it is hard to think that it was not enough from the time of the manufacturer's shipment, so I imagine that the seal was spilling and dropped at the time of packing work etc. . I think that you can thoroughly implement quality control. The goods themselves are easy to use and no problem.
This review is about item#45326601.
Equipment wiring, wiring connection to terminal block
5
From Japan
On 2017-12-17 22:40:25
Because it is connected to the terminal block with 2.5 mm spacing, it is compact and does not interfere with each other, just right. The core is in the center, the insertion port is also conical and the core wire is not caught, it is easy to use.
This review is about item#45326617.
Firefighting equipment construction
5
From Japan
On 2017-02-04 00:02:32
It is used when inserting a wire by plug-in terminal of fire-fighting equipment. I have been using the same thing for a while. It is handy because it does not enter the terminal unless it is this size.
This review is about item#45326601.
When wire is connected to the small terminal block on the board
4
From Japan
On 2016-09-30 12:57:32
I think the tip size is also good, and I think that it is a good article because the connection wire can be used widely.
This review is about item#45326617.
When wire is connected to the small terminal block on the board
5
From Japan
On 2016-09-30 12:13:32
The tip size is also good, making connection work easier.
This review is about item#45326617.
1