Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hexagon Head Bolts (Stainless Steel) All The Screw Threads

Hexagon Head Bolts (Stainless Steel) All The Screw Threads
Sales Price: 8.99 SGD
Review Rating: 4.42
12 Customer Reviews
5 star 8
4 star 2
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Machine assembly
4
From Japan
On 2017-04-28 16:58:41
Stainless steel bolt name Although it is expensive, it can be replaced with plated bolt because it is easy and satisfying.
This review is about item#45522836.
Purchase with replacement of bolt in rusty place
5
From Japan
On 2017-02-02 15:28:21
I decided to replace it with a stainless steel bolt because the bolt of the sprocket carrier of the motorcycle is made of steel and it is easy to stick to rust immediately. Because the so-called "fine pitch" is often used for motorcycles, it was quite expensive to buy at the town's home center, so I bought a cheap packed item based on Monotaro. It was about 60% of the price of the home center, but of course the bolt that remained unused was kept as a spare with the bolt on hand ♪ (laugh)
This review is about item#45522827.
During machine maintenance
5
From Japan
On 2016-09-01 15:42:10
It is a repeat. There is no problem in terms of price.
This review is about item#45522827.
Bolt tightening
5
From Japan
On 2016-03-28 20:10:01
good
This review is about item#45522811.
Agricultural machinery repair
5
From Japan
On 2015-09-08 05:43:05
I am satisfied because I can not get it at nearby stores.
This review is about item#45522836.
Fixed
5
From Japan
On 2015-08-13 22:28:48
Good because it is cheap
This review is about item#45522827.
For boat repair
5
From Japan
On 2015-05-13 07:57:26
It can be used as usual bolt. Since the M8 prepares several kinds of lengths, the small packs are saved.
This review is about item#45522836.
Fixing parts
2
From Japan
On 2014-12-02 18:06:42
I purchase it every time, but it is hard to use that the hexagonal part is 13 mm.It is not problematic in terms of goods but I think that it is easy to use if the hexagonal part is 12 mm or 14 mm.
This review is about item#45522836.
Installation of outdoor workpieces
3
From Japan
On 2014-05-13 13:20:16
The finish is also beautiful and the bolt itself is not inferior to the general one. However, it was regrettable that the plastic bag was split in the state that it arrived and it was scattered in the box.
This review is about item#45522827.
Used when installing outdoor air conditioner
5
From Japan
On 2014-02-11 16:10:58
Hexagon bolt of ordinary stain It is cheap The price is also purchased
This review is about item#45522836.
Used for fixing the mounting bracket of the control panel
4
From Japan
On 2013-09-19 15:48:30
Although there is no problem in terms of price with regard to use, if you purchase in small units, there is no indication in only simple numbers in simple packaging, you can not figure out how many mm of bolt is of course diameter, of course.
This review is about item#45522827.
Used as a substitute for dip pickled bolt.
5
From Japan
On 2013-05-31 17:33:07
If you look closely, there are fine scratches on the thread, but practically no problem at all. Anyway the price is attractive.
This review is about item#45522836.
1