Customer Reviews of Oil Seal
The reviews are automatic translation.
Showing 1 - 16 of 16 Reviews
As a seal material for switches

From Japan
On 2017-12-19 14:44:41
Image review and everything at all were different.
There is no point if there is no image of the product itself, not the representative image.
This review is about item#45986586.
bike

From Japan
On 2017-11-25 17:46:13
I can not use genuine oil seals in exchange for wheels other than genuine, this is the best choice for measurement, perfect
This review is about item#45987121.
Anchor winch

From Japan
On 2017-09-14 19:10:14
I used it for the anchor winch of the advancement (RES - 2012H). It is cheaper than orders from manufacturers.
This review is about item#45988065.
seal

From Japan
On 2017-08-31 16:21:34
Choice as a replacement part. There are no problems at the time of use.
This review is about item#45986595.
NSR 250 MC 21 for maintenance of the motorcycle

From Japan
On 2017-07-12 12:47:56
Dust seals (91254 - KV3 - 721) and 30 x 45 x 5 of the mag wheel of the NSR 250 MC 21 are replaced by the products of this manufacturer because it is out of the maker. Thickness is 1 mm thick, but there is no problem for use.
This review is about item#45988336.
Used for OH of cell motor

From Japan
On 2017-05-30 20:13:37
Oil leak has stopped with the same seal as the oil seal that is not part set.
This review is about item#45986796.
As a seal for the front wheel bearing of the Sky Way,

From Japan
On 2017-02-02 11:16:50
I purchased and replaced it as a substitute for genuine products. Of course there is no problem. Cheap finished, saved. (If there is compatible information ... it is too luxurious · · ·)
This review is about item#45988056.
Repair of small uniflow pump for electric dynamic spray

From Japan
On 2017-01-05 21:08:05
Since the grease was leaking to the motor side, it was repaired and repaired. Since the model number was stamped on the oil seal which was attached before, I was able to order this time with it as a clue. In this seal, the seal stated with the model number is affixed to the pouch, but the oil seal body is engraved with figures unrelated to the model number, why?
This review is about item#45987767.
Bearing end of motorcycle

From Japan
On 2016-01-28 16:02:45
Good
This review is about item#45986884.
Bicycle wheel bearings

From Japan
On 2016-01-21 20:31:33
The photograph and the actually delivered commodity are different, when seeing the illustration, the rubber is only inside, so it is not a perfect fake wake, but I want you to replace the photograph
This review is about item#45986787.
Instead of a washer

From Japan
On 2015-06-04 15:11:11
Since it was the use at the contact between the metal pipe and the metal surface, it meets the minimum specifications, but if you have rubber cushion on the contact surface it will be harder to slip, so please make it a product faithful to the published image I want to. Or, please correct the posted image to the actual thing, please describe it as chitin in the explanatory note.
This review is about item#45986875.
Vehicle maintenance

From Japan
On 2014-08-14 14:32:14
Only a small amount at a time, I will not purchase so it is useful in terms of price.
This review is about item#45987821.
Roller parts of belt conveyor

From Japan
On 2014-06-23 16:59:46
Since it is not used in a very precise place, there is no problem at all. Anyway it's cheap! It is probably a good shopping because if you buy a conveyor related part from a manufacturer purchasing it would probably price 2 ~ 3 times. Just a long delivery. Because ordering various sizes, depending on the thing, there are things of the missing item and there was an answer with the delivery date one month, and there were things canceled. It is perfect if all sizes can be delivered instantly ...
This review is about item#45987006.
For racing, use for front and rear wheels

From Japan
On 2014-04-25 14:20:51
☆ Although it is an additional evaluation to use for the race, since it is a single lip, the resistance at the start is considerably less than the original W lip. The tightening of the lip is also small. I think that it can be used enough for street use as it can be used even in harsh severe condition. The price is also profitable than purchasing genuine, strongly recommended!
This review is about item#45988171.
Machine maintenance

From Japan
On 2014-03-08 15:43:49
Equally equivalent to genuine products is very helpful! It is!
This review is about item#45988171.
1
Customers Who Viewed This Item Also Bought
<<
>>