Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Woodworking Clamp XP

Woodworking Clamp XP
Sales Price: 38.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Making 2 X 4 construction method huts
5
From Japan
On 2017-11-14 22:42:17
very good. Just drop it, the resin part will crack. I noticed after dropping off the other side (fixed side) of the grip and breaking it, but if this breaks it will be garbage because there is no handling of replacement parts. Is not it a waste? Can you just sell it ahead? What?
This review is about item#47324006.
Beat drop of bike tire
3
From Japan
On 2017-06-09 16:55:16
Slide type lock for angle adjustment is likely to come off. Tightening force is strong but grip strength is large, and work with both hands is necessary.
This review is about item#47323981.
Adhesive fixing of woodworking
5
From Japan
On 2017-01-27 14:36:08
Weight is also light, extremely easy to use, and the cost is also cheap so I would like to increase it in the future. (^ ^)
This review is about item#47324015.
Fastening until drying of adhesive
5
From Japan
On 2016-07-19 23:47:31
【Composition】 · Fixed part: other end point to fix the object · movable part: one end point pressurizing the object · release lever: small lever. Pressure can be relieved by pushing · Pressure lever: movable part can be moved to the pressurizing side at every stroke · H type regulating rod: black bar with fixed part and movable part 【Feel】 · It is solid and robust making · It can be used for temporary fixation at the time of bonding and fixation · Can not store compactly by dividing H type regulating rod · Oil application on H type regulating bar
This review is about item#47323997.
Temporary fixation of large processing member
5
From Japan
On 2015-06-22 14:43:13
Although I bought the biggest thing by mistake, it is supposed to be able to support 250 kg on fluke, fixed parts will not move at all. It is easy to work with high holding force, but as this clip is heavy, it is difficult to move with one hand to release the fixation with one hand and fix another part. Performance is the highest, a bit heavy, if the price is already cheap hundreds of yen, it is good enough that you do not have to buy a 150 kg model down one.
This review is about item#47323972.
1
Customer Who Viewed This Item Also Viewed
Clamp head
Click Clamp
Pipe Clamp
Woodworking Clamp
Handy Clamp
Quick change Micro
Tobi Chi Lang guard
K clamp
Uni-clamp, Flat