Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Plastic Bag

Plastic Bag
Sales Price: 17.60 SGD
Review Rating: 3.33
6 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
To garbage you do not want to leak to the outside absolutely
1
From Japan
On 2017-07-24 19:00:18
Since there was a thickness, the hole did not open, liquids and garbage came out, it was safe to use it. However, there were holes in 5 sets (50 bags) within 10 sets purchased the other day. The remaining 5 sets are not vacant, but since the holes were all in the same position, I think that the hole was vacant in units of lot. I thought that I would like to continue to purchase it if the product is a normal product with no holes, and I asked makers through Monotaro to ask if I can improve it in the future. However, there is no specific plan on the manufacturer side. It is very disappointing.
This review is about item#48936413.
To treat garbage including liquid
1
From Japan
On 2017-07-21 16:38:23
Because there was a thickness, liquid could not be leaked and was used with confidence. However, there were holes in 5 sets (50 bags) within 10 sets purchased the other day. The remaining 5 sets are not vacant, but since the holes were all in the same position, I think that the hole was vacant in units of lot. I thought that I would like to continue to purchase it if the product is a normal product with no holes, and I asked makers through Monotaro to ask if I can improve it in the future. However, there is no specific plan on the manufacturer side. It is very disappointing.
This review is about item#48936413.
Agricultural products
4
From Japan
On 2017-03-15 16:17:10
Transport storage such as potatoes, onions, taro, etc. It is strong because it is thick.
This review is about item#48936431.
Fish caught caught
5
From Japan
On 2016-08-06 18:00:34
There is thickness, it is very good without tearing.
This review is about item#48936413.
I used it for pickles
5
From Japan
On 2015-12-12 13:47:23
It is 0.1 in thickness. I did not go wrong anywhere in the neighborhood. You can use it without worry of breaking.
This review is about item#48936422.
Used when dirt throws out grueling garbage
4
From Japan
On 2015-09-11 14:47:28
It is a thick garbage bag. It is hard to break even with garbage with corners or hard garbage. I think that it is convenient to have 50 sheets entered.
This review is about item#48936431.
1
Customer Who Viewed This Item Also Viewed
Commercial Plastic Bag
For Special Thick Plastic Bags
Special Thick Plastic Bag
Commercial Thick Plastic Bags
For Special Thick Plastic Bags
Yo-Poly Bag, 0.1mm Thick
Plastic Bag
Plastic Bag
Plastic Bag