Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Vibration-Proof Rubber Block

Vibration-Proof Rubber Block
Sales Price: 16.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Improvement of vibration of air-conditioner outdoor unit
5
From Japan
On 2016-08-18 18:35:40
1. According to the manufacturers, due to the mold of the indoor unit, noise and vibration of the outdoor unit occurs 2. We requested the disassembly / cleaning at the manufacturer factory and improved it, but there was noise and vibration, the wall surface was also resonating and it was the range of consideration 3. The antifungal method seems to be air-conditioned at about 32 degrees, but since it is an air conditioner over 15 years ago, it is only up to 30 degrees 4. So, we are endeavoring for sleeping (male hormone secretion) with cooling operation at 30 degrees (during work), noise and vibration reduction of gel damper and melatonin production tag of vitamin B6 5. As an aside, growth hormone is within 3 hours after sleep onset, male hormone is from 22:00 to 26:00, and 6 g of glycine is also used to prevent halfway awakening
This review is about item#49066534.
Absorption of impulsive sound by door opening / closing
5
From Japan
On 2016-05-17 17:46:00
It was more than expected effect. Impact sound has decreased to the level that it wants it to be so. I am satisfied. I think that it was better if there were variations on the size.
This review is about item#49066534.
Measures against noise of air conditioner outdoor unit
5
From Japan
On 2016-02-20 09:47:43
I was bothered by the noise of the outdoor unit at bedtime, but I felt no sound at all! It was good to buy ^ ^
This review is about item#49066552.
Inverter air conditioner Noise and vibration reduction of outdoor unit
5
From Japan
On 2015-12-14 17:15:51
It was effective in a fairly wide frequency band.
This review is about item#49066595.
1
Customer Who Viewed This Item Also Viewed
Anti-Vibration Pad
Air Spring WF Type
Foam Rubber, Black
Cushion Rubber
CLAMPING KITS
FLAT WASHER
PUNCH PRESS SETS
STEP BLOCKS
STEP CLAMPS