Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of File Handle

File Handle
Sales Price: 5.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
File file
3
From Japan
On 2018-03-26 00:55:30
This time, I bought all kinds (five kinds) which sell screw-in handle of Tsubosan with monotalrow. Wood is originally imported with numbers written in the butt, in Tsubosan it is managed by SML. The size of this SML hole is the same with wood and rubber. I think that the hole is large with respect to the size of the handle. This rubber made S is the size you want to use at 150, and the flat 150 can be used as usual. The corner sticks to the body and stops. Triangle is impossible. was. The notation for size is not wrong because it is not written for 150, but it is a shit sorry. If you want to correspond to all 150, 200, 250 Although the price will be doubled, I think that it can be dealt with because it is the smallest screwed type of Hellobbe. If you want to use a thin file with a large grip, the snap-on screw-in type has a smaller hole, but the price is more than five times the price. As a good story about it, if you can request from Tsubosan from the monotarou, it is better for Wood to tell that the import supplier is a manufacturer that is making things with thinner holes, so you should import it.
Rasping
5
From Japan
On 2016-08-10 11:39:41
As you screw in, the handle acts like a dice and screws are formed on the file itself. I sometimes want to use a file as well as use it, so it is convenient to remove the handle easily. When reinstalling it, it is good to turn it in the reverse direction and tighten from the sunken place.
This review is about item#58100865.
When steel is polished
5
From Japan
On 2016-07-11 20:53:36
It is easier to use and removes so it can reduce inventory count.
This review is about item#58100865.
For the hands of a file
5
From Japan
On 2015-05-21 07:49:46
Although it was not a file of a screw type, I used it while wearing it by pounding it firmly. The feeling of grasping is easy to use fitted to the hand moderately. It is a plain item, but it is a very important part as it is surprisingly very good feeling.
This review is about item#58100865.
1
Customer Who Viewed This Item Also Viewed
File design
Iron File
Handle
Single line
File design
Wave rasp (wave rasp)
Single line
File design
Quick cut Varito