Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Angular Contact Bearing

Angular Contact Bearing
Sales Price: 2.99 SGD
Review Rating: 4.33
3 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Conveyor repair
From Japan
On 2018-01-13 13:37:19
I am using it without problems. It was saved to be able to purchase on the net.
This review is about item#58098031.
From Japan
On 2014-10-23 14:31:27
I used it for the rear of a handmade cart. Because the ears are attached, extra welding etc can be deleted, it was very helpful. The price was also cheap and good. It seems to be unsuitable for high-speed rotation etc., which requires high load, but it was a level that I could use with no problems like me like me.
This review is about item#58098013.
It is a replacement bearing for agricultural harvesting truck tires.
From Japan
On 2013-06-20 18:19:03
When replacing the bearing of the working truck, since it is a four wheel tire, a total of 8 bearings are required at the two bearings on both sides. Until now, the selling price of the shop that I had purchased was very high, and when I purchased the number of one car, I was able to purchase the original dolly. For this reason, it was a place where we were struggling to replace parts. I saw your parts this time and thought it was this, I ordered it. However, half were concerned about whether price and size fit, and half were uneasy. However, thank you for delivery with a short period after ordering. I immediately felt half sentiment and replaced the parts, the sizes also agreed, I recently felt the appreciative of MonotaRO, not happy. Even if it is a small, trivial thing to many people, I am fortunate if you can supply it. From now on, I will use your company as a consumer and as a fans fan. I feel that it is a company that has never existed.
This review is about item#58098047.