Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Aluminum Flat Head Nut Packed

Aluminum Flat Head Nut Packed
Sales Price: 11.99 SGD
Review Rating: 4.86
7 Customer Reviews
5 star 6
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
To fix sheet metal together
From Japan
On 2018-02-23 11:45:52
I used it to fix sheet metal together. Unlike the rivetter, it is convenient to fix the screw. In the photograph of the product page the jaggedness of the slip is attached to the root of the riveter, Attention is necessary because jaggedness was not attached to this product.
This review is about item#58383613.
Production and repair of automobile parts
From Japan
On 2017-02-02 18:25:30
At the same time I bought a thing of pop rivet fastener company, but it seems to be exactly the same thing. Both markings are written as POP. (It is not a mistake in seeing TOP) It may be an OEM item. I tested both products properly by caulking both products properly, but both things are the same or both can be used properly. I do not sell small blind nut M3, so I think it is valuable.
This review is about item#58383613.
Nut mounting on steel plate
From Japan
On 2016-02-01 23:38:04
Because it is made of aluminum, it is easy to caulk. It is better not to exceed the specified tightening torque of the bolt. I'm rich in size so I would like to purchase again.
This review is about item#58383717.
Mounting on Aluminum Car Port
From Japan
On 2015-05-19 22:49:56
I installed it in the aluminum carport frame. By attaching a round hook (screw type), we try to hang sunshades and others. If summer is over it will remove the sunshade, but use the hook as it is. It may not be able to withstand a large load because it is aluminum, but now it is comfortable to use.
This review is about item#58383674.
Aluminum sash
From Japan
On 2014-10-23 20:40:16
The screw hole that had been opened in the aluminum sash was enlarged and it was not useful to change the size of the screw head so it is useful for using the same size. Because it has some thickness, I use it somewhat modified.
This review is about item#58383631.
Car parts installation
From Japan
On 2014-08-08 19:08:20
It is convenient for the reinforcement of the spoiler and the stay of the license plate installation.
This review is about item#58383647.
For car interior use
From Japan
On 2013-05-10 22:52:49
It was used for interior installation of a light van. I used a steel plate with an appropriate hole and capped using M5 bolt. Using the electric impact screwdriver makes working easier but if you use the same bolt too much, the bolt broke in about 4 times so I think that you can work without waste before replacing the bolt before it breaks.
This review is about item#58383665.
Customer Who Viewed This Item Also Viewed
Hand nutter
Nut Rivet
Pop Nuts
  • Pop Nuts
  • 4.99 SGD
  • 4.666670(3)
LOBSTER Hand Nutter
Steel Knurled Nut
Flat-Head Rivet Nut
Rivet Nut
POP Standard nut Small flange AFH SF (aluminum) (pack product)
Blind nut
Flange Nut Pack
Paper string