Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mold Knob K-2195

Mold Knob K-2195
Sales Price: 1.99 SGD
Review Rating: 3.71
7 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Volume box
5
From Japan
On 2017-11-12 22:17:49
The lighting condition is a little cheesy, but the usability was quite good.
This review is about item#8626125.
Equipment production
1
From Japan
On 2017-10-02 14:35:18
Although it is satisfactory not to get in the way of being small as a knob, I bought two but the set screws were not attached to one. I am allowed to use it with an attractive short delivery date, but because the reply to the inquiry of the exchange is late, it is one star.
This review is about item#8626134.
As a knob of the potentiometer.
2
From Japan
On 2016-10-14 17:04:04
I am thankful that a set screw is attached.
This review is about item#8626134.
Oven range controller knob
5
From Japan
On 2016-08-23 16:10:02
The oven range timer controller has been revived with this product. Thank you.
This review is about item#8626116.
Speed ​​control of the inverter
5
From Japan
On 2015-11-30 22:01:04
Use of hex wrench (enamel set) is very helpful. I want an inscription that fits this knob.
This review is about item#08626116.
Used for volume knob of vacuum tube amp.
5
From Japan
On 2014-03-10 20:09:32
You can use it from before and it is extremely easy to use. For those of size L, I'd like you to put a bigger zag of the spigot of the shaft hole. Since the tightening nut of the volume is protruding, it seems that it floated a little when it was installed.
This review is about item#08626107.
Used as a control knob of mechanical mechanism
3
From Japan
On 2014-02-11 14:26:39
At the time of carrying in, there are things that the attached stop screws are detached and need attention. In case of missing the male screw, the M3.5 screw is outside the standard and can not be purchased separately. The use of such external standards should be avoided and may be referred to as a defective product.
This review is about item#08626125.
1
Customer Who Viewed This Item Also Viewed
For Rv30 Series Potentiometer Miti Equipment
RA30 Series Potentiometers, Wire Wound
Mold Knob K-5010
Mold Knob K-66
Mold Knob K-1
Mold Knob K-3
Mold Knob K-90
Mold Knob K-2605
Mold Knob K-2901
Mold Knob K-5380-A
Mold Knob K-6
Mold knob K-75
Metal Knob K-59
(25230) Starter relay
Tachometer Indicator
Mold Knob K-2800
Mold Knob K-8