Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Nephron Ptfe Tube Tombo No.9003-Ptfe, Mm Size

Nephron Ptfe Tube Tombo No.9003-Ptfe, Mm Size
Sales Price: 2.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Fishing trick
5
From Japan
On 2017-07-30 12:07:16
This tube is passed through a jujube sinker (middle through hole), and it helps to eliminate the roots of sinkers. If it is 20 to 30 cm on the Harris side of No. 18 or No. 20, it will also protect the line, and if the PTFE tube is moderately inevitable, the coefficient of friction will be extremely small so that it will not split even if rubbing against rough reefs . This product is useful because it can select finely the inside diameter according to the thickness of the line. If I want a greed, I would be happy if you could offer it a little cheaper ...
This review is about item#2949703.
Maintenance of 3D printers
5
From Japan
On 2016-06-05 14:11:14
Friction resistance of the filament of the 3D printer is very low, even if R is tight, it goes to Sulul. PTFE is high, but it is the strongest resin in various aspects.
This review is about item#59713997.
I insert a soft wire tube in this tube and use it for electrical connection.
3
From Japan
On 2015-03-05 18:30:53
Because it is a naflon, there is no choice, but if you put a little force it will bend and it will not return to its original bending scratches will be attached, it will be stiff with slight flexibility to make it slightly flexible and bendable, but?
This review is about item#02949825.
Used in the experiment
5
From Japan
On 2014-11-13 13:08:59
Variation of size is also good, I frequently purchase. Although it is very handy, if there is further demand, it will be saved if you can shorten the number of days to delivery.
This review is about item#02949685.
1
Customer Who Viewed This Item Also Viewed
PTFE Tube, 1 M Roll
PFA Tube, 1 M Roll
PTFE tube (10 m winding)
PFA Tube, 10 M Roll
Yodoflon PTFE Tube 6x4
Fluorine Resin Tube, PFA
Naphron (R) BT tube (mm size)
PFA Micro Tubes
PFA Tube
PFA Tubing, mm Size
FEP Tubing