Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Sanace Acfan

Sanace Acfan
Sales Price: 28.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Heat of breaker
4
From Japan
On 2017-06-08 21:18:05
Good usability. It is very useful to lower the heat of electric appliances.
This review is about item#8584125.
Used as cooling fan for audio system
4
From Japan
On 2017-04-18 15:16:50
As for the exhaust heat of the amplifier, I purchased it with particular emphasis on quietness, but as expected, it was awesome quietness. There is not much air volume, but it was within the range of assumption, so I do not feel the problem in particular at present. However, one of four of the first purchases was clearly noisy and it was NG, so I bought one new one. Although it is a quiet AC fan, it seems that there are variations in manufacturing.
This review is about item#8584125.
As an exhaust fan of a signboard
5
From Japan
On 2016-08-18 11:33:40
It is very easy to use because it is small and sound quiet. It is good that the price is not so high.
This review is about item#8584125.
Heat exchanger inside the furniture
5
From Japan
On 2016-04-03 20:13:05
Very quiet and stable
This review is about item#08584125.
For AV rack heat dissipation
5
From Japan
On 2015-08-19 23:53:04
The front glass door has almost no evacuation spot on the rear side. Since the amplifier and BD recorder housed in the AV rack are hot, they are mounted on the AV rack rear plate for the exhaust heat. Although the static pressure and the air volume were sufficient, and the noise was uneasy, it surprisingly dissipated heat and it was very quiet. Noises are very satisfying at a level which is not at all mind even at midnight. Used for extrusion in 50 Hz area.
This review is about item#08584125.
1
Customer Who Viewed This Item Also Viewed
Fan Motor
AC Axial Fan R87F
AC Fan Motor
Fan Motor
AC Fan Motor
AC Fan Motor
AC Fan Motor
Plug Cord
Cooling Fan SanACE Filter Kit
AC Axial Fan R87T
Standard Sanace Fans
Finger Guard
SanACE Fans
ACDC fan 9AD type
AC Fan Motor
Cooling Fan
AC Fan Motor
AC Fan Motor
AC Fan Motor