Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Carbide Hole Saw Long Type

Carbide Hole Saw Long Type
Sales Price: 37.99 SGD
Review Rating: 3.40
5 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
When processing parts
1
From Japan
On 2016-05-28 14:05:18
Used for drilling SS material t 20 mm. An abnormal noise occurs when opening about 5 mm. After confirming, one chip was dropped, which caused other chips to be damaged. I think that there was no problem with cutting oil as well as feeding amount. After all, the work ended in a state where it was not possible to process even one new purchase.
This review is about item#62837336.
It is drilling of iron plate.
5
From Japan
On 2015-09-11 17:15:01
I bought two hole saws, so it got messed up. The carbide long saw was the thicker steel plate. I'm out of stock.
This review is about item#62837381.
Maintenance
5
From Japan
On 2015-02-27 13:10:05
It was a very good product for the price.
This review is about item#62837345.
Metal Processing
1
From Japan
On 2014-12-25 17:05:19
When we drilled about 10 holes, all chips were gone.
This review is about item#62837327.
Drilling into stainless steel BOX
5
From Japan
On 2014-10-07 18:03:47
In ordinary bimetallic hole saws, it will burn easily if you do not pay too much attention, but cemented carbide will not bleed continuously even if it is used, it is a big help.
This review is about item#62837345.
1