Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pipe Saddles

Pipe Saddles
Sales Price: 13.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
The base of the antenna element
4
From Japan
On 2017-11-09 21:28:16
It is mounted as a base pedestal of the antenna element, and it fits the pipe diameter and it is solid. It is saved if there are various kinds of dimensions of φD, but I want you to increase the type.
This review is about item#86840022.
When RF tube is fixed
5
From Japan
On 2017-09-09 20:40:24
Saddles such as metallic piping and the like which can be fixed at one point have been used since before, but there was only one manufactured by Miguro Industry, which can be fixed at one point for PF piping . There are color variations of each PF tube, so it will be appreciated, but I am somewhat saved a lot (about 20 units) for myself who do not always use the least number of lots a little.
This review is about item#86840047.
Air conditioning drain
5
From Japan
On 2017-07-15 16:10:51
It can also be used for PVC Kan. If you want to raise the height, cut the rubber plate under the base to match the dimensions, I use it spreading. Since one screw hole can be used, work can be done quickly.
This review is about item#86840056.
Electric piping construction
5
From Japan
On 2017-06-20 16:39:32
Although the unit price per piece is higher than one or both saddle bands, it looks beautiful after construction and it is also good for enforcement so I use it again and use it.
This review is about item#86840056.
Electrical construction
5
From Japan
On 2015-08-07 14:35:28
It is best to be able to use PF tube and VE tube and it is best to easily remove saddle at incoming line. The price aspect is high but the workability is good.
This review is about item#86840056.
1
Customer Who Viewed This Item Also Viewed
TS Coupling Straight Type
Spacer for PF / VE dual saddle
Normal Bend
VE both saddle pedestal
VE saddle attached
Spacer for VE saddle
Terminal Bushing
Pf Pipe Connector, G Type
No. 2 Connector
VE Single Saddle
FV rack (for the general shape steel)