Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Clamp Lever

Clamp Lever
Sales Price: 6.99 SGD
Review Rating: 4.33
6 Customer Reviews
5 star 3
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Fixing the tool post of the table turning lathe
4
From Japan
On 2017-11-22 02:55:37
The function is not a problem at all. Although it is not in comparison with other products, I felt that the paint film was somewhat weak. I just peeled off just by touching a knife. I do not need to search for a hex wrench and it is useful. I bought Orange, but it was also good for looking up as an accent.
This review is about item#68097635.
Drilling machine for drilling machine
5
From Japan
On 2017-10-17 15:45:58
I am using it to fix the vise of the drilling machine, it is useful when changing the position finely.
This review is about item#68097574.
Telescopic frame parts
5
From Japan
On 2017-03-29 16:32:34
I posted a misunderstanding as something different. This is very satisfying because it is familiar to the hand well and easy to turn.
This review is about item#68097565.
As a part of the telescope mount
3
From Japan
On 2017-03-29 15:42:14
Unlike photographs, what I was sent to me felt that the end of the lever was thin and difficult to enter power.
This review is about item#68097565.
Machine work
5
From Japan
On 2016-03-14 18:35:45
Lathe, milling machine and various other knob screws etc are replaced with clamps. It is possible to tighten securely and change the clamping position, so safety and working efficiency are rising.
This review is about item#68097626.
Machine tool slide lock
4
From Japan
On 2015-04-21 15:13:45
Since it is a part that is used frequently, the material of the screw part is S45C, so we can expect high durability. However, it is still in sight as it is still in use. I am very satisfied with the price. Although it is not limited to this product, the clamp of the female thread would like the thread part a little more in length. Most products have thread length of 7 mm. With M6, only 5 or 6 bars are chewed with a pitch of 1 mm. If it is a male screw, there are also longs ...
This review is about item#68097565.
1
Customer Who Viewed This Item Also Viewed
Clamp Lever KF
Clamping Lever
Plastic Ball
Clamp Lever
Clamp lever (female thread) KF
Clamp Lever (Bolt)
Clamp Lever
Knurled knob flat
UAC aluminum cabinet handle
UAF aluminum handle
LDF clamp lever (female screw)
Plastic clamp lever (female thread) VF
LECF Minipura clamp lever (female thread)