Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Industrial Abrasive Pad No.180

Industrial Abrasive Pad No.180
Sales Price: 28.99 SGD
Review Rating: 4.60
15 Customer Reviews
5 star 10
4 star 4
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 15 of 15 Reviews
Cutlery rust remover
5
From Japan
On 2017-08-08 16:03:33
It is a high-quality item that exceeds the imagination, it can be knife-edged with this product if it is a knife which polished the rough polite carefully.
This review is about item#75862464.
Coating film polishing
5
From Japan
On 2017-05-01 18:31:31
It is not inferior to famous manufacturer products. It is easy to use.
This review is about item#75862464.
Exterior wall cleaning (tile)
4
From Japan
On 2017-03-25 14:47:10
Compared with Kenmaron, decided by price, consumption is fast, but COSPA is expensive.
This review is about item#75862464.
Rusting off
4
From Japan
On 2017-03-15 16:14:56
Easy to use with reasonable size and coarse grain. You can cheap. It was used for rust removal in general.
This review is about item#75862464.
Matte hairline finish of frp, foot attachment of small parts etc.
5
From Japan
On 2017-03-09 16:43:42
When adding a foot to a part with small unevenness of about 1 mm in depth, it is better to move the part by placing it on the table than moving the file. This # 180 is moderately hard and has a high fiber density, and when the grid is rougher than this, the fiber density is sky and it gets caught when it is attached with a foot such as a screw head and rust removal, and it gets caught and when the grid becomes finer than this It is too soft and stuck, easy to break and brittle, and in the first place grids of # 320 and above can be purchased even in kitchen utensils, and even in Homsen you can buy large and small varieties, so I will use it a lot, but I try not to be so much concerned. As an indication of hardness, this green is # 300 - 400 in kitchen utensils and it is about the contents of bread, this is the ears of bread bread. Also, with a little hardening thing, you can attach feet without wood to square corners at right angles, frosted, remove dirty. As a further trick, it is possible to add rust removal feet inside the pipe by attaching an epoxy adhesive to the bit tip which became unnecessary such as a drill or electric screwdriver, so if you cut it small and stab it, what you sell for that purpose is Since it will cost you a few hundred yen, you can make ten pieces with this one piece. The one with a rough grid than this is a skusca and the adhesive flows and it has few adhesive surfaces, so do not hold it. The fine grid is so soft that it can be wrapped and used, but the cutting force is also weak, at high speed foil balance is difficult to get out, so it tends to fall apart.
This review is about item#75862464.
Rust removal
4
From Japan
On 2017-01-05 14:44:18
Rust removal of the foundation before painting can be made unexpectedly easy, it can be easier than rubbing with a wire brush, etc. It will not hurt.
This review is about item#75862464.
To the processing under work !!
5
From Japan
On 2016-07-12 21:15:23
I worked on paper up to this point, but the Scout Bright was easy and easy.
This review is about item#75862464.
Polishing
5
From Japan
On 2016-05-01 06:03:40
Hope of marketing # 80. (Aspire)
Cleaning the cement
5
From Japan
On 2016-02-04 17:01:27
Work was easy because lightly dirt falls down
This review is about item#75862464.
Stainless steel HL finish
3
From Japan
On 2015-12-10 19:36:28
It is a bit thin, but I think I can use it. I think that it would be better if there is more price difference between Ken Maron and making it thicker a little.
This review is about item#75862464.
I use it for removing water scrap attached to a stainless steel plate.
5
From Japan
On 2015-11-05 17:44:48
Every time, we purchase. Purchasing with coupons is even more advantageous!
This review is about item#75862464.
Polishing
5
From Japan
On 2015-08-13 22:18:26
I feel it is a little soft. I want to use it if there is a hard one at # 60 to # 120
This review is about item#75862464.
Remove rust
5
From Japan
On 2015-07-03 22:59:29
It is used for rust removal of iron and copper. I feel that rust can be taken more efficiently than sandpaper of the same count.
This review is about item#75862464.
Polishing of stainless steel
4
From Japan
On 2015-01-17 12:29:59
There is no particular problem
This review is about item#75862464.
Polishing operation
5
From Japan
On 2014-04-17 15:38:50
Thickness is thin, but you can use it normally. 80 # 60 # etc .. release.
This review is about item#75862464.
1
Customer Who Viewed This Item Also Viewed
Sanding Sponge,
Sanding Sponge,
HP-7447
Abrasive Hand Pad
Migakiron
Sink drain plug basket
Polishing Scrub Brush
Abrasive Hand Pad Box
Scotch-Brite super stubborn
Ken maron (1 piece)