Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of OILES Gliteon SE Bush

OILES Gliteon SE Bush
Sales Price: 1.99 SGD
Review Rating: 3.25
4 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Repair of scooter
2
From Japan
On 2016-10-30 15:13:33
As soon as the part was sent it confirmed it, the dimensions are the same but the material was a resin type look. As a matter of fact, it was a part of the idle gear holding of the cell motor, so I decided to install it. I thought that it was full feeling that it would not work. There was no particular problem.
This review is about item#75825224.
For machine maintenance
5
From Japan
On 2016-08-01 16:32:47
It is used as a bearing collar, but it has been adapted.
This review is about item#75825224.
For bolt inner diameter adjustment
1
From Japan
On 2014-11-24 01:28:24
The size was just right, but it was broken as "Pakipaki" when trying to remove it after temporary loading and it did not become usable.
This review is about item#75825276.
Scooter kick spindle bearings
5
From Japan
On 2014-10-24 15:16:49
I hope there is 12 mm in the L dimension.
This review is about item#75825242.
1
Customer Who Viewed This Item Also Viewed
Drymet LF Bush
OILES #80 Bushing
BB Bush
DDK05 Bush
TMDB OILES TAFMET
Oiles Cermet M
OILES Bearing
OILES No.300 Bushing
Gliteon F Bush
Gliteon SE
Bearing DBB
Die Best DBS 02 Bush DBS
OILES fiber CFC FW Bush
OILES 2000 bush
OILES Flange Bush