Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Screw Catching Magnet

Screw Catching Magnet
Sales Price: 5.99 SGD
Review Rating: 3.00
7 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 2
1 star 2
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Car maintenance
1
From Japan
On 2018-02-02 22:31:03
It is no good at all. It will not be used. I would like you to put an easy-to-understand picture such as an actual picture from the inside diameter display.
This review is about item#75189642.
During maintenance
2
From Japan
On 2018-01-19 14:56:14
I wonder if it is considerably weaker than I thought. I plan to purchase a different type.
This review is about item#75189642.
Used when exchanging keys
5
From Japan
On 2018-01-11 18:10:32
The parts of the key are small, and since the exchange of the keys is also at night, it is very handy as it is easy to eliminate the screws removed.
This review is about item#75189633.
Electrical work in general equipment installation etc.
1
From Japan
On 2017-12-18 14:02:27
I attached it to the driver, but I returned it because the screws are not sticking at all. Even cheap items purchased at home center with the same driver even though the screws stick together Even if you install this product it is completely defective product.
This review is about item#75189642.
For screw tightening work
5
From Japan
On 2017-06-14 15:46:19
I was looking for something to use with the driver attached. I also like magnetic design and very strong design. I fell into a narrow place. It is also ideal for picking up screws.
This review is about item#75189642.
Air conditioner construction, home appliance maintenance
2
From Japan
On 2015-08-14 16:35:39
I tried to install it to a very popular ball grip driver of Bessel, but the shaft diameter 0.1 mm driver can not fit thick. It was "No way ...". Let's purchase after checking the shaft diameter of the driver you are using.
This review is about item#75189642.
Tighten the screw with a screwdriver
5
From Japan
On 2015-03-26 20:13:06
Previously, I did not know such a product, but I was struggling with iron screws, but this is convenient. I wish I had used it earlier. I'd like to attach it to all the drivers I have.
This review is about item#75189642.
1
Customer Who Viewed This Item Also Viewed
Mug Fit
Magnet Bit Holder
Magnetic Screw Catcher
Magnetic Catch
Magnetic Screw-Holder
Magnetic Screw Catch
Magnetizing Holder
Magnet Bit Holder
Screw Catch & Adjuster
Magnetic Catch
Screw Holding Bit
Magnetic Catch
Magpita
  • Magpita
  • SUNFLAG (SHINKI MFG)
  • 4.99 SGD
SF Pitattokun
Ultrashort mug catch
Screwdriver Magnetizer Demagnetizer