Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Screw Catching Magnet

Screw Catching Magnet
Sales Price: 7.19 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
work
4
From Japan
On 2017-04-14 16:59:36
It is convenient although screws do not fall, but it is reasonable.
When using the driver
4
From Japan
On 2017-01-05 14:44:03
Very convenient to purchase immediately on the net. I was impressed that there is such a convenient one
This review is about item#75189651.
Wiring work
5
From Japan
On 2016-06-13 08:30:07
Although the screws of the equipment inside the control panel are small and it may be dropped at the time of wiring, there is also magnetic force and there is no worry of dropping, so it can be used with confidence
This review is about item#75189651.
Control panel production
5
From Japan
On 2015-12-07 17:59:55
Easy to work as screws do not fall
This review is about item#75189651.
We are using it attached to the bit of the charge driver.
5
From Japan
On 2014-06-23 22:19:43
Even when using the magnet bit, it got irritated and it got annoyed. After wearing this, the sticking became better and the thing dropping the screw was reduced less. Perhaps it was good to be a little more powerful. I think that it is such a thing because it is a mini size.
This review is about item#75189651.
1
Customer Who Viewed This Item Also Viewed
Mug Fit
Magnet Bit Holder
Mag Dry Power, Dry Bar Magnetizer
Magnetic Catch
Magnetic Screw Catcher
Magnetic Screw Catch
Magnetizing Holder
Magnet Bit Holder
Magnetic Catch
SF Pitattokun
Magnetic Catch
Magnetic Catch
Ultrashort mug catch
Screwdriver Magnetizer Demagnetizer
Magpita
  • Magpita
  • SUNFLAG (SHINKI MFG)
  • 4.97 SGD