Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stubby Screwdriver

Stubby Screwdriver
Sales Price: 5.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Purchase as a mobile tool
4
From Japan
On 2016-12-10 21:39:04
I bought it as a portable tool of a folding bike. It is compared with VESSEL stubby driver 270 W, but VESSEL = 45 g / L = 68.3 mm and 5 g lightly by 5 mm for ANEX = 40 g / L = 73.6 mm. Although inserting / removing a bit is hard, the attached bit can be long without problems. VESSEL is loose, but bit is short and it is hard to grab. Bessel felt well for a long handle of the handle but it is a place where opinions are divided according to taste here. If light aim is to be carried for the purpose of mobile, ANEX will raise the army if it is the first. For VESSEL 270 W for normal use, ANEX 1580 for mobile use.
This review is about item#75189956.
For in-vehicle tools
5
From Japan
On 2016-05-23 15:42:44
I use it with a replacement screwdriver bit (long) of the truss. The grip is short because it is a stabilizer, but because the diameter is enough, the torque is transmitted from a bad driver. I think that the grip surface is elastomer, so it seems that the dirt falls bad, but it is good to not slip.
This review is about item#75189956.
Machine maintenance
5
From Japan
On 2015-03-26 16:24:24
The retention of the pit was loose to feel good and easy to insert and remove. (Bissel's sturdy but it was too stiff and needed pliers) Design is cheap but price is also cheap so there would be no choice. It is sufficient for small portable use.
This review is about item#75189956.
1
Customer Who Viewed This Item Also Viewed
Stubby Ratchet Screwdriver
Stubby Driver
Single mixing faucet
2WAY high soft stubby
Replacement stubby driver set
2WAY stubby driver
Replaceable Stubby Driver
8way Universal Driver