Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of T-shaped Hex Wrench

T-shaped Hex Wrench
Sales Price: 19.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Drain removal of motorcycle carburetor
4
From Japan
On 2017-12-19 16:50:43
It is used for the drain of the large two-wheel carburetor of Kawasaki. Because genuine tools are pretty expensive, substitute here. The length was quite long, and it arrived without problem even for large two-wheelers. It is 3mm that I bought and it is considerably thin, so it will cause a lot of screwed ends. It is natural, but it is not suitable for high torque. However, we have been very satisfied because we have found only a long and affordable product so far.
This review is about item#75303593.
I use it to tighten the inner hexagon bolt in the back place.
5
From Japan
On 2016-05-30 13:59:21
It is handy because it is light and easy to use, so it does not take up space.
This review is about item#75303593.
In a deep place
5
From Japan
On 2015-06-15 19:52:44
I was satisfied with the impression I used because I was looking for thin and long things. Since I do not use it many times a year, I thought that it would be nice to have a cheaper one with T-shaped metal bare, without "a high-grade acetate resin handle that feels good". .
This review is about item#75303611.
1
Customer Who Viewed This Item Also Viewed
ATL T Type Long Hexagonal-Bars Wrench
Ball Point T Type Wrenches
T Long Hex Key Wrench
T-Shaped Hey Key
T-Handle Hex Wrench
Tapered head T-shaped hex wrench
T-type hex wrench Long type
T-shaped Hex Wrench
Hexagon T- handle
T-shaped Hex Wrench
T Hex Wrench
Ball point , T- handle
Ball point , T- handle
Hexagon T- handle