Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Cobalt Drill Bit

Cobalt Drill Bit
Sales Price: 3.99 SGD
Review Rating: 5.00
2 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
For compensating set
5
From Japan
On 2016-07-28 16:47:57
One (1 mm in diameter) in the set purchased over 20 years ago was broken at work mistake, so I bought it as a supplementary one. It is exactly the same length as the original one, and it fits perfectly in the case. It was written with the same material HSS. I am always very sorry for the variety of Monotaro's assortment.
This review is about item#75366261.
Drilling for tapping
5
From Japan
On 2014-02-04 01:41:03
When tapping bolt holes of 8 mm - 1.25, you can usually pilot holes with a 6.8 mm drill, but in case the other is made of aluminum, it is slightly bigger, there are times when the bolt is slightly rattled when you put the bolt. In such a case, if you drill a prepared hole with this 6.7 mm drill, it is very convenient. However, it is a bit tight to put a tap, so be careful and it is also essential to use plenty of tapping oil.
This review is about item#75366837.
1
Customer Who Viewed This Item Also Viewed
Cobalt Masamune Drill(HSCO-M42)
HSS Drill
G straight drill
HSS Straight Shank Drills
HSS Straight Shank Drills
Pack drill
Cobalt straight drill