Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hose Quick Connector

Hose Quick Connector
Sales Price: 8.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Cut out the hose part where the hole is empty, and use the normal part joint.
5
From Japan
On 2018-05-04 15:29:24
I did not have to throw away the normal part of the usable hose. Efficient use up to the endurance limit of the hose is economical. Although it is a one-touch attachment / detachment, there was no water leakage from the joint portion, and the effect was outstanding.
This review is about item#75753054.
Extension of hose during car washing
5
From Japan
On 2018-04-14 15:21:25
It was easy to install and made very good shopping without water leakage.
This review is about item#75753054.
Hose extension
5
From Japan
On 2018-04-09 19:16:21
It is used for extending the hose on the water supply side of the high pressure washer. I was satisfied.
This review is about item#75753054.
Extension of the hose at the veranda at home
5
From Japan
On 2015-08-10 22:01:21
The length of the hose was insufficient, and I bought a hose relay. Even women could easily connect two hoses! After using it, I thought that it would have been nice if I had purchased it earlier without water leakage from the seams. It was easy to use, the price was cheap, it was too early to arrive, so when I have something again I think I will ask Monotaro.
This review is about item#75753054.
When using the Super J nozzle of order number 05870287 purchased earlier, joint the root part of hose.
1
From Japan
On 2015-07-15 19:21:13
Since there was a notation of correspondence with pressure hose, I installed the male side at the tip of the hose that connected the super J nozzle and used the female side attached to the hose near the faucet of the tap. The first time we opened the faucet by about a third was able to be used without problems, but as we increased the amount of water to near the full open, the joint melted and the water gushed out and the clothes got drenched. It is doubt whether it can be said that it corresponds to withstand pressure hose.
This review is about item#75753054.
1
Customer Who Viewed This Item Also Viewed
Garden Hose Connector
Snap Taps
PT1/2 Connector
Faucet Hose Connector
Intermediate joint
Hose Rotation Joint
Water Tap Fitting
Water Hose Coupler
Multi Socket
Faucet Hose Connector
Watering Nozzle,Pachitto
Rotate Hose Joint
Joint Hose Nipple
Hose Joint