Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Welding Shield Glass

Welding Shield Glass
Sales Price: 189.99 SGD
Review Rating: 4.00
8 Customer Reviews
5 star 4
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
To the price price ...
2
From Japan
On 2018-02-01 00:15:48
Osaka soul is several times better. I can see it sharply, but the back of my eyes hurts.
This review is about item#75900291.
welding
5
From Japan
On 2017-08-22 08:57:54
It was awesome. I think that it was good to buy though the price was expensive.
This review is about item#75900291.
During arc welding
5
From Japan
On 2017-02-13 14:36:53
When field welding, arc welding with one hand, it is easy to check the position of the arc start, it is easy because there is no mistake of arc striking the base material. The number of useless back steps has also decreased, and the results of X-ray inspection are also excellent. If you want a greed, you should strengthen a little more. Because it is surprisingly close to the position of the weld line and face as it is on site welding.
This review is about item#75900291.
Welding operation
4
From Japan
On 2016-10-15 13:13:47
This is the second purchase. It's not bad because it's a reasonable amount. There seems to be no such thing as light blurring. However, it seems to be weak against heat. The liquid was darkened by heat when I took the face too close by the glass shielded lens, but it got relieved after returning to the original after a while when it cold. I would like to have a product that is resistant to heat if possible.
This review is about item#75900291.
Welding of rebar bar
3
From Japan
On 2016-06-15 19:20:33
Since it is installed on the sunglasses to secure visibility, light rays from the side enters and eyes hurt with ultraviolet rays. I think that it is easy to use if it becomes possible to block the ray from the side.
This review is about item#75900291.
Welding operation
5
From Japan
On 2014-10-07 19:34:00
I used the light shielding filter of "Osaka soul" before, but I do not have it. I was replacing every year. I bought the one of "Yamamoto Engineering" for the first time so I do not yet understand the good or bad. I think that reaction to welding light is fast. I will purchase this if I have good in the future.
This review is about item#75900291.
welding
3
From Japan
On 2014-06-04 16:45:29
It would be great if it could be used for Tig welding ...
This review is about item#75900291.
Steel welding etc.
5
From Japan
On 2014-03-23 17:03:25
It is easy to see and work comfortably.
This review is about item#75900291.
1
Customer Who Viewed This Item Also Viewed
Welding Mask
Welding Helmet, LCD
Liquid Automatic Shade Welding Helmet Jidoumen
Welding Plate
Welding Helmet, LCD
Welding Shield Glass
Welding Shield Glass
Welding Cover Plate
Promise
  • Promise
  • STAR ELECTRIC MANUFACTURING (SUZUKID)
  • 229.99 SGD
  • 4.000000(1)
Rainbow mini set