Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Squeegee

Squeegee
Sales Price: 9.99 SGD
Review Rating: 3.67
6 Customer Reviews
5 star 2
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Mirror water droplet blowing etc.
3
From Japan
On 2017-09-24 05:00:35
It is repeat (second time). I used it for 1 year and a half. Rubber is not bad at all, but drainage has become worse. The new one is a nice feeling.
This review is about item#88131915.
Cleaning the garage window
5
From Japan
On 2017-04-24 14:36:32
Moisture can be taken cleanly with preeminent rubber sticks often eaten. It is easy to twist the return of reciprocating work because it also has easy handle. It is a gem that is also appreciated in price.
This review is about item#88131915.
Utilized for taking moisture after bathing in the bathroom
5
From Japan
On 2016-09-29 17:49:05
I was able to remove moisture easily. There is more effect than a ventilator.
This review is about item#88131915.
Draining of a bath
3
From Japan
On 2016-09-28 02:05:51
no problem. I can use it normally. I think that it is suitable for price.
This review is about item#88131915.
Water drop removal of bathroom wall
2
From Japan
On 2014-07-17 08:53:37
I expected it for professional use, but rubber is too hard for the purpose of use, it can not drain well and it will bounce. It seems that the usage like scraping off dirt, such as glass, is suitable. I gave up using. After this, I bought a car wiper type one, but it was almost satisfactory usability.
This review is about item#88131915.
Cleaning the window glass
4
From Japan
On 2014-06-24 19:44:36
I think that it is good in cost performance.
This review is about item#88131915.
1
Customer Who Viewed This Item Also Viewed
Handy Wiper
200mm Window Squeegee
450mm hand wiper
Glass squeegee
Handy Squeegee 24cm
Stainless Steel Squeegee
Condor water squeegee
Handy Glass Wiper