Customer Reviews of Stainless Steel Squeegee
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Window glass cleaning

From Japan
On 2018-03-12 08:00:18
Until now, I wiped it off with cloths as usual, but I wiped it off with this wiper in one shot, making cleaning easier.
This review is about item#88131933.
During cleaning

From Japan
On 2018-03-06 11:28:32
Purchased because there is no store selling nearby.
Especially the quality is not a problem.
This review is about item#88131942.
Clean windows and glasses and mirrors in the bath, cleaning the walls

From Japan
On 2018-02-24 22:37:27
Easily windows can be easily wiped simply by spraying a glass wipe detergent on the window glass and dropping it from the top down with this wiper
, I bought the second one this time. It is easy to use.
This review is about item#88131933.
Window cleaning

From Japan
On 2018-01-16 14:36:34
The width is also 30 cm and the handle is thick and easy to handle.
There is no uneven wiping.
This review is about item#88131933.
Window wipe

From Japan
On 2017-01-30 16:12:38
When you hold the grip, it is easier to use as it is easier to apply force to the index finger.
This review is about item#88131967.
For bathroom

From Japan
On 2016-12-06 19:14:03
I tried using it, it was preeminent draining. Although it was a little expensive, I bought it was a correct answer.
This review is about item#88131933.
Mainly glass cleaning

From Japan
On 2016-10-29 07:52:48
It was a bulky good product because it was detachable. Easy to handle even if you are unfamiliar.
This review is about item#88131933.
Cleaning the window glass

From Japan
On 2016-06-12 06:05:33
I have purchased it at home center until now but this product can finish neatly without leaving a wipe left.
This review is about item#88131942.
1