Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Sleeve-All Anchor

Sleeve-All Anchor
Sales Price: 17.99 SGD
Review Rating: 4.27
11 Customer Reviews
5 star 7
4 star 2
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Machine installation. Because there is work that does not use the number, I think that 10 retailers are very convenient.
5
From Japan
On 2018-05-17 09:26:42
From now on, please increase divide sales. Even if it becomes expensive, I think that it is better not to waste.
This review is about item#75960866.
Machine installation
5
From Japan
On 2017-09-08 20:07:34
I used it as a pedestal for installing heavy machinery. The price is reasonable and satisfying, but it may be glad if there are 4 units as well. For people who rarely have opportunities to use it will be in vain if 10 pieces are left over
This review is about item#75960954.
Ceiling installation
5
From Japan
On 2017-01-17 18:55:26
I am satisfied that I can firmly install it. Durability is unconfirmed.
This review is about item#75960884.
Fixation of installation
1
From Japan
On 2016-12-26 10:47:13
Even at the time of 15% off Osaka spirit is raised, it is meaningless if it is higher than the manufacturer's rose item (Taitoanka) × 10.
This review is about item#75960936.
For construction
5
From Japan
On 2016-11-18 18:10:47
Moderate 10 pack sets, affordable price satisfaction.
This review is about item#75960866.
A signature
4
From Japan
On 2016-04-28 19:48:41
It was the same as other manufacturer's products and it was able to be used without problems
This review is about item#75960902.
Anchor embedding in concrete
3
From Japan
On 2016-04-09 21:54:54
I drilled with a 10.5 mm drill and driven, but I am dissatisfied. You should drill with 11 millimeter drill and drive
This review is about item#75960936.
Block fence
5
From Japan
On 2016-03-27 03:20:34
I have not used it yet, but it seems that there is no particular problem.
This review is about item#75960902.
Anchor claw
5
From Japan
On 2016-03-02 17:39:31
It is cheap and the goods are also solid so it is very good.
This review is about item#75960893.
Baffle installation in manhole
5
From Japan
On 2015-03-05 18:52:39
Suddenly you need a short size and purchase. The delivery schedule was earlier and it was in time for the construction term.
This review is about item#75960893.
I am using it for installing outdoor workpiece
4
From Japan
On 2014-06-16 20:16:27
You can use it just like steel. Because the price is expensive, consider the cost when using it
This review is about item#75960902.
1
Customer Who Viewed This Item Also Viewed
Stainless Screw Anchor
Tight Anchor Stainless Steel
All Anchor, Steel, Pack Product
C Type Anchor
Sleeve-All Anchor SC
Tight Anchor, Stainless Steel
Anchor Bolt
Tight Anchor, Hot Dip Galvanizing
With 10-mm All Anchor