Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Forstner Bit

Forstner Bit
Sales Price: 16.99 SGD
Review Rating: 4.38
24 Customer Reviews
5 star 16
4 star 5
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 20 of 24 Reviews
It is used for grooving when attaching a hinge of a cabinet of a kitchen hanging cabinet.
5
From Japan
On 2018-03-16 16:49:44
Well, it is easy to use and cut. In woodworking work, I think that it is an indispensable tool for making furniture etc.
This review is about item#86928116.
For processing in woodworking.
4
From Japan
On 2018-03-08 09:10:36
It is easy to handle and excellent in cutting ability. Cutting (cedar wood) Scratch tends to cling to the cutting edge, so please improve it.
This review is about item#86928107.
For wood processing
5
From Japan
On 2018-03-06 19:10:49
It was sharp, inexpensive, sophisticated with high performance. I would like to ask again. Thank you very much.
This review is about item#86928152.
Woodworking
4
From Japan
On 2018-02-12 15:46:43
I changed the bit and gradually enlarged the hole, I was able to do a good job as I expected.
This review is about item#86928091.
On the pillar of a cypress
5
From Japan
On 2018-02-04 09:54:23
By cutting it slowly, I could pierce a beautiful hole.
This review is about item#86928125.
Used to drill the door knob part
5
From Japan
On 2018-01-22 15:01:11
I used it to drill a door knob on a solid door. The size is also perfect.
This review is about item#86928204.
Drilling
1
From Japan
On 2017-08-11 20:07:16
I bought it a little cheaper than Star M wave cutter and thought that it was better than the home center made in China. Made in China when you see the product. Like the home center, the blades were not sharply cleaned. I tried to drill, but heat and smoke come out, but the cut is not good. Another size Star Mu purchased together was out well. This is good if it is 980 yen in the home center.
This review is about item#86928107.
Digging of furniture hinges
5
From Japan
On 2017-08-10 14:51:13
Depending on the material, there are products that produce white smoke, but it is easy to use and is easy to use.
This review is about item#86928082.
Bamboo, polishing after drilling of wood
1
From Japan
On 2017-07-31 14:51:31
There is no effect at all. Even if it rotates, the polishing power can not be seen. It may be used for soft wood ...
This review is about item#86928055.
Work digging into wood
5
From Japan
On 2017-07-03 05:23:31
Easily, I could dig a very clean hole. In continuous work seems to be cutting cutting power with a slight heat sag, It was necessary to dissipate heat, but I did not feel a problem.
This review is about item#86928116.
"Sharpness good" · · · There is further hope
4
From Japan
On 2017-06-19 08:37:00
I am using it for woodworking, but the point that the frictional heat does not rise because the sharpness is good is excellent. However, since the stroke of our drilling board is 80 mm, we can only open the depth to the position of the chuck with small diameter (φ 30 mm or less). At φ32 mm or more, the chuck also enters the opened hole and the maximum depth is possible. I think that a bit with a small diameter needs more length. Because it is a sharp sharpness, I told you a bit of complaints. Someday I would like to arrange a bit of longer if it is sold.
Wood burying process of wood
5
From Japan
On 2017-02-18 08:17:28
It also shows its sharpness against sharp, sharp clade nodes. Cospa is also nice.
This review is about item#86928021.
○ Hole machining
4
From Japan
On 2017-01-17 21:55:11
Since a hole drilling bit of 29 mm in size was not found, it was possible to drill in a clean state and there was no drop of the cap and it was good.
This review is about item#86928091.
Drilling
5
From Japan
On 2017-01-12 22:02:55
You can drill a hole neatly without burrs. We also plan to purchase the size.
This review is about item#86928116.
Resin bearing mounting
5
From Japan
On 2016-12-15 20:10:49
Installation of resin bearings Groove engraving was easy and easy.
This review is about item#86928091.
Woodworking drilling processing
5
From Japan
On 2016-07-03 23:33:38
I was saved because I could buy the necessary size right away. I could cut without problems.
This review is about item#86928116.
Drilling of wood etc.
3
From Japan
On 2016-03-29 17:19:37
I used it in the drilling machine but it felt like sharpness fades quickly. I made a touch-up with a diamond rapper, but it is a place where doubts remain with hardwood etc .. Although I feel that there is no ginger in price.
This review is about item#86928046.
○ Hole machining
4
From Japan
On 2016-01-16 22:02:11
The bottom is level and can be beautiful. The stability of the round bar is also good.
This review is about item#86928055.
Making a dining chair
5
From Japan
On 2015-09-21 21:23:10
Good
This review is about item#86928021.
Piping
5
From Japan
On 2015-08-05 16:54:59
It was saved because there was not a size of Fosunabit in the nearby home center. I thought it was very convenient.
This review is about item#86928213.
1 2
Customer Who Viewed This Item Also Viewed
Power Pit No.1
Super Woodworking Drill
No.1 short bits
No.5008 Triple Cutter
Drill, Bamboo
Driver Bit
Zagurikiri
No.600 Wave Cutter
Brad Point Bit
Hinge cone A (front screw)
Hinge A-B (Triangle)
Triple cutter
Short Driver Bit